RealSense Support

I am struggling in calibrating realsense rgb camera intrinsic parameters

Comments

6 comments

  • MartyX Grover

    Hi Dannguyen  You can list the intrinsics and extrinsics details for all of the sensors using the rs-enumerate-devices tool by using the launch command rs-enumerate-devices -c ('c' stands for 'calibration').

    https://github.com/IntelRealSense/librealsense/tree/master/tools/enumerate-devices 

    You can query the intrinsics and extrinsics of the sensors with more precision by using the rs-sensor-control tool.

    https://github.com/IntelRealSense/librealsense/tree/master/examples/sensor-control  

    In regard to calibrating the intrinsics ... the normal version of the official Dynamic Calibrator tool only calibrates extrinsics.  There is however an OEM version of the software that can calibrate both extrinsics and intrinsics.  It is supplied as part of the $1500 USD OEM Calibration Target system.

    https://store.intelrealsense.com/buy-intel-realsense-d400-cameras-calibration-target.html 

     

    0
    Comment actions Permalink
  • Dannguyen

    Hi MartyG, thanks a lot for your quick help.

    About RGB intrinsic value, do you know how to validate the intrinsic value collected after "Targeted calibration"? Since I used chessboard calibration for a conventional camera to get intrinsic of RGB sensor, but the result is not repeatability - especially for focal length and distortion coefficients. 

    Appreciate your help.

    Regards,

    Dan

    0
    Comment actions Permalink
  • MartyG

    I made an edit to my opening comment after first mentioning RGB calibration with Targeted Calibration, as I saw that you were trying to calibrate intrinsics and the normal version of the Dynamic Calibrator only calibrates extrinsics (the OEM version of the tool is required for intrinsics calibration).  My apologies for that.

    0
    Comment actions Permalink
  • Dannguyen

    Hi MartyG, thanks for your help about camera calibration tools, as I understand, will calibrate the accuracy and repeatability for depth image. I have also do the Dynamic calibrator, and visually see the image is less noise. But do you know any numerical method to validate the calibration output is good? I mean Intel only give the illustration for what is "good" and "not good" depth map, see below, but I curious about how much accuracy is added, or how to tell which intrinsic value is better?

    0
    Comment actions Permalink
  • MartyG

    As well as the Dynamic Calibrator tool, you can also use an On-Chip Calibration tool that is built into the RealSense Viewer program to test the camera and provide a 'heath check' value for the calibration.  There is a Tare tool in the Viewer too for improving depth measuring accuracy.  Both tools can be found in a menu under the More option at the top of the Viewer's options side-panel, and Intel have published a white-paper guide to use of On-Chip Calibration and Tare.

    https://dev.intelrealsense.com/docs/self-calibration-for-depth-cameras 

     

    I would recommend using the Dynamic Calibrator when you need to perform a thorough and robust calibration of the camera's imager components, and use On-Chip Calibration for more regular checks. 

    There is also the option of testing depth image quality and receiving feedback about it (such as the amount of error) using the Depth Quality Tool

    The normal version of the Dynamic Calibrator tool only calibrate extrinsics because it is extrinsics that have the most effect on depth quality.  Users of the OEM version of the tool have the option of calibrating intrinsics too, though that system is aimed at engineering departments and manufacturing facilities, and 99% of RealSense users will not require it.

    0
    Comment actions Permalink
  • Jakob

    Hi Dannguyen

    Thanks for having a look at the Calib.io Camera Calibrator software for intrinsic calibration.

    There are a couple of important points to consider when performing camera calibration. I recommend having a look at our best practices article: https://calib.io/blogs/knowledge-base/calibration-best-practices

    In your particular case, the calibration board is barely tilted. Tilt (foreshortening) is necessary to constraint the focal length estimation. This is the main reason you are getting a large uncertainty on the focal length parameter.

    For distortion coefficients, please note that the higher order model you are using requires a good amount of observations (images). Also, these parameters are not entirely independant. Different combinations of them can actually describe very similar distortion fields.

    Best regards

    Jakob, Calib.io 

    0
    Comment actions Permalink

Please sign in to leave a comment.