RealSense Support

Does the depth scale of the D435 change with each run, each frame, or is it fixed?

Comments

4 comments

  • MartyG

    Hi Radhwan Sani  The depth scale on the 400 Series cameras remains fixed at the default value of 0.001 (meters) unless deliberately changed.  Even when changed, it remains constant until the next time that it is manually changed.  

    The depth measurement in meters is obtained by multiplying a 16-bit pixel depth value (uint16) with a range between 0 and 65535 by the depth scale value.  For example, 65535 x 0.001 = 65.535 meters.

    1
    Comment actions Permalink
  • Radhwan Sani

    Thank you MartyG,

    Our experiment involves measuring the distance in a close-range e.g. 2 meters.

    Should we keep using the default depth scale value, for higher accuracy?

    Thanks

    0
    Comment actions Permalink
  • MartyG

    The default depth scale value is fine for that distance.  If you seek optimum depth accuracy then a depth resolution of 848x480 is optimal for the D435 model.  Also, you could try using the High Accuracy visual preset configuration.

    https://dev.intelrealsense.com/docs/d400-series-visual-presets 

    0
    Comment actions Permalink
  • Radhwan Sani

    Thank you MartyG

    0
    Comment actions Permalink

Please sign in to leave a comment.