RealSense Support

D435i not found with old firmware.

Comments

1 comment

  • MartyG

    Hi Sean Forrester Roelofs  The D435i was introduced a year after the D435 and so has a minimum firmware.  I believe that the earliest available one that supports the D435i is 5.11.4.  You should of course update to the most recent firmware though.

    If the camera is not appearing in the RealSense Viewer, you can try updating the firmware using the rs-fw-update firmware update tool.  This tool includes a camera recovery mechanism if the camera is not detectable by normal means.

    https://dev.intelrealsense.com/docs/firmware-update-tool 

     

    If you are using Windows, you can find a pre-built version of the tool in the SDK's Tools folder. (C: > Program Files (x86) > Intel RealSense SDK 2.0 > Tools).  

    0
    Comment actions Permalink

Please sign in to leave a comment.