RealSense Support

The resolution of the camera image is only half

Comments

3 comments

  • MartyG

    On your Ubuntu system, if you are using the RealSense Viewer program then please check in the Post-Processing section of the options side--panel (found under the Stereo Module category) whether a filter option named  Decimation Filter is enabled.  If it is on (shown by a blue icon next to it) then click on the blue icon to change it to red (off).

    0
    Comment actions Permalink
  • 819765928

    Well, it's true.Actually, it's OK with my code.I changed my camera from D415 to D435i,but I didn't notice the difference in the field of view between the RGB and the depth of the d435i.So,I using the RealSense Viewer found out about this. 

    0
    Comment actions Permalink
  • MartyG

    The Viewer has a range of post-processing filters enabled by default, but when writing your own application there are none enabled and you have to deliberately add filters into your program.  This is why there can be clear differences between an image in the Viewer and an image generated with your own code.

    It is worth mentioning that on the D415, the field of view size of depth and color sensors is the same.   On the D435 models the depth FOV is larger than the color. Depth gets sized to the color FOV size when aligning depth to color.

    0
    Comment actions Permalink

Please sign in to leave a comment.