RealSense Support

calibration board for d400?

Comments

1 comment

  • MartyG

    The official calibration chessboard for the 400 Series cameras can be downloaded as a PDF from the link below.  The calibration image is the whole of page 1, which you print off and then point the camera at.

    https://dev.intelrealsense.com/docs/dynamic-calibration-print-target 

    It is worth making sure that you know though that the calibrate_extrinsics.py script isn't the same thing as the Dynamic Calibrator or On-Chip Calibration.  It is for calibrating a T265 and a D345 together (for example, when they are attached together on a 3D printed mount).

    0
    Comment actions Permalink

Please sign in to leave a comment.