RealSense Support

LIDAR Accuracy for less than 3 meter length

Comments

1 comment

  • MartyG

    Hi Praveensidharthhtic  I do not have an estimate for accuracy at 3 meters.  As a rough-estimate rule though, on the 400 Series stereo depth cameras the accuracy over distance is calculated as being less than 1% of the distance of the camera from the object.  That equates to around 2.5mm to 5 mm at 1 meter distance, like on the L515 model.

    Given that expected accuracy at 1 meter is 2.5 mm minimum, 2mm at 3 meters may be very difficult to achieve.  The best accuracy may come from using the new D455 stereo camera model, as it has improved accuracy over distance by a factor of 2x compared to the D435.  So the D455 has the same accuracy at 6 meters that the D435 does at 3 meters.  You may be able to attain some additional improvement by using a camera configuration option called High Accuracy which alters the balance of the camera's various settings in favor of better accuracy, whilst trading off other aspects such as image fill-rate.

    Ultimately though, I cannot offer any guarantees of a particular accuracy range before purchase, especially as other factors such as environment and lighting may also influence the amount of error.

    0
    Comment actions Permalink

Please sign in to leave a comment.