RealSense Support

Skeletal tracking behind desk or with partial viewport

Comments

3 comments

  • MartyG

    Hi Matan  Traditionally, performing skeletal detection on people in unusual poses such as laying down, or when "off screen" from the camera's view, has always been difficult.  Microsoft's Kinect 1 dealt with the problem of non-visibility of joints with algorithms that predicted where body joints should currently be if not visible.  Developers also had to create custom algorithms to handle poses that the SDK software did not support by default (such as "if the user is detected to be in Pose A + Pose B, they must be in Pose C").

    Modern skeletal SDKs such as Cubemos Skeleton Tracking SDK are better these days though at automatically working out where joints are if the body is occluded (for example, by walking behind another person).  If you play the Cubemos demo video and go through it carefully by pausing / unpausing with the spacebar, you can see glimpses of how Cubemos handles occlusion situations.  For example, on the horse riders, Cubemos predicts the joints of both legs and displays them even though one leg is hidden from the camera angle's view on the other side of the horse.

    https://www.youtube.com/watch?v=PENY6Q24c6A 

     

    1
    Comment actions Permalink
  • Matan

    Thanks for the broad perspective reply. Happy to hear more from community members. In particular in my case there is no need to guess where the feet are ... they are just not interesting for my scenario and I wonder how much does the recognition of the upper body, mostly arms and hands, head, is adversely affected when the lower body is occluded! 

     

    This might really help prior to my own experiments and choice of RealSense hardware model!

    0
    Comment actions Permalink
  • MartyG

    Cubemos seems to treat joints individually.  Parts that cannot be calculated disappear whilst the rest of the joints remain, and invisible joints instantly reappear as soon as they can be calculated again.  In the image below where a person walks in front of another person, their lower body temporarily disappears but their upper joints remain.

     

    1
    Comment actions Permalink

Please sign in to leave a comment.