RealSense Support

D435i SLAM on Raspbian buster /raspberry pi 4

Comments

13 comments

  • MartyG

    Do you get the same result if you do not use $ROS_VER and instead enter the single line below, please:

    sudo apt-get install ros-melodic-realsense2-camera

    0
    Comment actions Permalink
  • A Dhesi2

    yes I tried that as well and it still said unable to locate package ros-melodic-realsense2-camera

    0
    Comment actions Permalink
  • MartyG

    Do you have an active internet connection?

    0
    Comment actions Permalink
  • A Dhesi2

    yes

    0
    Comment actions Permalink
  • MartyG

    There is an alternative guide in the link below to installing Librealsense and ROS on a Pi 4 with Raspbian Buster that you could try:

    https://eleccelerator.com/wiki/index.php?title=Raspbian_Buster_ROS_RealSense 

     

     

    0
    Comment actions Permalink
  • A Dhesi2

    ok I will try this thank you, I will let you know how it goes. Thanks for the help.

    0
    Comment actions Permalink
  • A Dhesi2

    I followed the instructions on the site to get kinetic yesterday and it still didn't allow me to get ros-kinetic-realsense2-camera.

    0
    Comment actions Permalink
  • MartyG

    I researched this case extensively from the beginning to look for new possibilities to follow, but did not find much.  My feling is that at this point, the best path to follow may be:

    1.  Download a pre-made SD card image of Librealsense for Raspberry Pi 4 that Intel created and write it to an SD card.  It is available from the link below.  

    https://dev.intelrealsense.com/docs/open-source-ethernet-networking-for-intel-realsense-depth-cameras#section-2-3-preparing-the-sd-card 

    This should provide a reliable installation of librealsense on Pi 4 to build ROS upon.

    2.  Build ROS from source code using Method 2:

    https://github.com/IntelRealSense/realsense-ros#step-2-install-intel-realsense-ros-from-sources 

    0
    Comment actions Permalink
  • A Dhesi2

    When doing method 2 i got the ros-package ddynamic_reconfigure and proceeded with catkin_make clean but then it gives a cmake error saying I need dynamic_reconfigure, nav_msgs, nodelet, bondcpp and pluginlib so i then go those in the same manner as ddynamic_reconfigure. But then it says instead of using catkin_make clean use catkin_make_isolated so i did the aswell. but this gives me a new error saying pluginlib is a package with an unkown build type and so i'm at a bit of a dead end. 

    0
    Comment actions Permalink
  • MartyG

    The eccelerator guide had problems with pluginlibs too and offered this advice about their error: "This happened when I tried to use a prebuilt version of libboost 1.58 instead of building my own version. Seems like the prebuilt version was built using an older compiler and so the symbols don't match. The solution is to build libboost 1.58 from scratch with the new compiler, or switch the entire build to the old compiler".

    Building ROS on Pi 4 seems to be rather difficult, to be honest!

    0
    Comment actions Permalink
  • A Dhesi2

    in the instructions for ROSberry for setting up kinetic there is instructions that account for this I think sudo apt remove libboost1.67-dev
    $ sudo apt autoremove
    $ sudo apt install -y libboost1.58-dev libboost1.58-all-dev

    etc...

    On https://github.com/IntelRealSense/realsense-ros#step-2-install-intel-realsense-ros-from-sources it says to make sure all dependencies are installed, this is where i'm having problems.I keep running catkin_make clean and catkin_make_isolated to see what dependency i'm missing and then cloning the url's into catkin_ws/src in the same way i got dynamic_reconfigure and ddynamic_reconfigure and then using git checkout 'git tag | sort -V | grep -P "^\d+\.\d+\.\d+" | tail -1'. Do you have any information or guides about this section or the proper way of getting these dependencies (I only first started using a Pi earlier this year so idk if my questions might be a bit basic.)

    Edit: At the bottom of http://wiki.ros.org/ROSberryPi/Installing%20ROS%20Kinetic%20on%20the%20Raspberry%20Pi there is a section about adding released packages Im going to put in realsense2_camera, imu_filter_madgwick, rtabmap_ros and robot_localization then try run roslaunch realsense2_camera opensource_tracking.launch

     

    0
    Comment actions Permalink
  • MartyG

    Apologies for the delay in responding further.  I would speculate that the travis.yml dependencies that the Method 2 instructions refer to are the sudo apt-get instructions in the link below:

    https://github.com/IntelRealSense/realsense-ros/blob/development/.travis.yml#L23 

    0
    Comment actions Permalink

Please sign in to leave a comment.