Cubemos SDK installation problem : Depends: libboost-log1.65.1 but it is not installable
I encountered the following error during Cubemos skeleton tracking SDK installation when executing the command :
"sudo apt-get install ./cubemos-SkeletonTracking_*.deb" insie the extracted folder v2.3.1" I My system is ubuntu 16.04. What are the other packages that I need to install?
"""
Note, selecting 'cubemos-skeleton-tracking-sdk' instead of './cubemos-SkeletonTracking_2.3.1.6cffde4.deb'
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:
The following packages have unmet dependencies:
cubemos-skeleton-tracking-sdk : Depends: libboost-log1.65.1 but it is not installable
Depends: libboost-filesystem1.65.1 but it is not installable
Depends: libboost-program-options1.65.1 but it is not installable
Depends: libboost-regex1.65.1 but it is not installable
Depends: libboost-chrono1.65.1 but it is not installable
Depends: libboost-date-time1.65.1 but it is not installable
Depends: libboost-atomic1.65.1 but it is not installable
Depends: libssl1.1 but it is not installable
E: Unable to correct problems, you have held broken packages.
"""
-
In case the installer package that you downloaded has problems, there is a complete Cubemos installer file also available on my Google Drive that you could try.
https://support.intelrealsense.com/hc/en-us/community/posts/360039440173/comments/360010657054
-
I'm having the same problem with Raspbian 10 (buster) and the SDK. I tried installing from the one via the google drive above because the download appears to be broken from the original website.
It still says I need all those dependencies. Is there something else I can do, or a good guide out there for getting the realsense SDK working on a pi 4?
-
Hi Shane Huston If you are having problems with installing the Cubemos Skeleton Tracking SDK that the installer file cannot solve: the Cubemos skeleton SDK is a product of the Cubemos company and not an Intel product. Please send your question to Cubemos support by visiting the link below and starting a web-chat with a support operative by clicking on the 'Got any questions? I'm happy to help' button in the label's bottom corner.
If you need a quick way to set up the RealSense SDK on a Pi 4, Intel provide a pre-made Pi 4 SD card image and accompanying instructions at the link below:
Please sign in to leave a comment.
Comments
3 comments