Pip3 error with pyrealsense2
Hi
I want to install pyrealsense2 in ubuntu 32bit using python 3.6, but i get an error :
Could not find a version that satisfies the requirement pyrealsense2 (from versions: )
No matching distribution found for pyrealsense2
Thanks for the help
Regards
-
Odroids have ARM processors, and ARM devices will not work with pip install. This is because the pip packages are designed for x86 and x64 processors, and ARM is not 'x' architecture.
You can build Librealsense from source code and include an instruction to build the Python bindings along with it at the same time. Here is an example CMake statement that includes the Python bindings. It uses the "backend" method of installation, which requires an internet connection but is not dependent on Linux versions or kernel versions and does not need to be patched:
cmake ../ -DFORCE_RSUSB_BACKEND=true -DBUILD_PYTHON_BINDINGS:bool=true -DCMAKE_BUILD_TYPE=release -DBUILD_EXAMPLES=true -DBUILD_GRAPHICAL_EXAMPLES=true
Alternatively, if you do not want to rebuild Librealsense then you can build the pyrealsense2 wrapper from source code.
-
Hi Mhmh6086 Did you build the librealsense SDK on the external hard drive using the Ubuntu on there, please?
-
Hi sorry to reply late, We didnt need the external any more and now need to use the camera in pc with ubuntu 18.04. we have built the librealsense SDK but the camera cannot be detected . for you to know the same hardware of the camera is working fine with windows pc.
I appreciate your help
-
Hi Mhmh6086 Which method are you using to install librealsense on Ubuntu please - DKMS distribution package or building from source code? Thanks!
Package method
https://github.com/IntelRealSense/librealsense/blob/master/doc/distribution_linux.md
Source code method
https://github.com/IntelRealSense/librealsense/blob/master/doc/installation.md
-
Hi Mhmh6086 If you experience problems with both of the above methods of building librealsense in Ubuntu then you could try a build method called RSUSB. It requires an internet connection to carry out the installation process but it is not reliant on Linux versions or kernel versions and does not require patching. It is therefore an excellent tool for diagnosing whether a problem is related to the Linux kernel if the problem does not occur when using the RSUSB installation method.
The link below provides instructions for installation using the RSUSB method. Where the instructions mention 2.36.0, substitute that for whatever librealsense version that you are building from source code.
https://github.com/IntelRealSense/librealsense/issues/6845#issuecomment-659540316
You may also find the link below useful when considering the differences between the RSUSB installation method (known previously as libuvc) and conventional kernel-based patching.
https://github.com/IntelRealSense/librealsense/issues/6368#issuecomment-636320762
-
Hi i built it using https://github.com/IntelRealSense/librealsense/issues/6845#issuecomment-659540316 . but still device not connected.
-
Hi Mhmh6086 The Viewer's error message reports that your RealSense installation has udev rules missing. These are rules that govern the handling of devices. Can you try the procedure below please?
STEP ONE Refresh the local packages cache
sudo apt-get update
STEP TWO Run the command below to install the udev rules
sudo apt-get upgrade/install librealsense2-udev-rules
-
Thank you for the reply .
the step 2 gives an error :
Reading package lists... Done
Building dependency tree
Reading state information... Done
E: Unable to locate package librealsense2-udev-rulesAlso the realsense is located in /usr/local/lib/librealsense2.so
Thanks in advance for your help :)
-
The Unable to locate package error has happened before with the 32-bit version of Ubuntu, if you are still using the 32-bit version that you were at the beginning of this case.
-
I wonder if it is resulting from your current librealsense installation being built from source code with the backend method according to your post from 4 days ago but the sudo apt-get upgrade command is part of the distribution package installation method.
You could try going to the librealsense root directory and running the udev script command from the librealsense source-code installation guide:
./scripts/setup_udev_rules.sh
-
Thank you very much for your patience. I would expect a backend type installation to work immediately without camera detection problems such as this. It is a situation where it is sometimes best to just remove the whole librealsense installation and start again with installation from the beginning.
Also, make sure that any previous installations of librealsense are removed, as you reported that you had tried both types of build (package and source code) after switching computers.
https://support.intelrealsense.com/hc/en-us/community/posts/360048315774/comments/360012860614
After that comment, you then performed an RSUSB type installation. So potentially, three different build methods have been attempted on the same PC. So you may have better results if there is only one installation (the RSUSB one) on your computer.
-
Thank you for your reply .
No i only have the one installed following https://github.com/IntelRealSense/librealsense/issues/6845#issuecomment-659540316.
so im going to try again the patching one.
-
when i run the code to capture the frame , I got the error :
pipe_profile=pipeline.start(config)
RuntimeError: Couldn't resolve requests############################################################################################
Im working on Ubuntu 18.04.5 LTS (GNU/Linux 5.4.0-47-generic x86_64).
i followed link : https://github.com/IntelRealSense/librealsense/blob/master/doc/installation.md#prerequisites.
im going to specify the steps that i have done as follow :
1- sudo apt-get install libglfw3-dev libgl1-mesa-dev libglu1-mesa-dev
2-sudo apt-get update && sudo apt-get upgrade && sudo apt-get dist-upgrade
3-git clone https://github.com/IntelRealSense/librealsense.git
navigate to librealsense root
4-sudo apt-get install git libssl-dev libusb-1.0-0-dev pkg-config libgtk-3-dev
5-sudo apt-get install libglfw3-dev libgl1-mesa-dev libglu1-mesa-dev
6- ./scripts/setup_udev_rules.sh
7- ./scripts/patch-realsense-ubuntu-lts.sh
8- mkdir build && cd build
9- cmake ../ -DFORCE_RSUSB_BACKEND=true -DCMAKE_BUILD_TYPE=release -DBUILD_EXAMPLES=true -DBUILD_GRAPHICAL_EXAMPLES=false
10- sudo make uninstall && make clean && make && sudo make install
-
If you are using -DFORCE_RSUSB_BACKEND=true then you do not need to do any patching, as the dependencies are installed over an internet connection. The RSUSB process is described in the instructions in this link:
https://github.com/IntelRealSense/librealsense/issues/6710#issuecomment-650611442
If you intended purposely to build librealsense with the patching method then do not include -DFORCE_RSUSB_BACKEND=true in the CMake build instruction.
-
i Did and this is the error and warning :
2020-09-23 12:12:07,662 WARNING [default] Could not open device command transfer failed to execute bulk transfer, error: RS2_USB_STATUS_IO
Traceback (most recent call last):
File "CameraCapture.py", line 17, in <module>
pipe_profile=pipeline.start(config)
RuntimeError: No device connected -
Here is a comment relating to a case where this error occurred:
https://github.com/IntelRealSense/librealsense/issues/4768#issuecomment-526817879
Please sign in to leave a comment.


Comments
46 comments