RealSense Support

D435 crashes on Intel NUC8th generation, Ubuntu 16.04, ROS Kinetic.

Comments

3 comments

  • MartyG

    Hi Howoncheong  The RealSense Viewer and RealSense ROS wrapper are not meant to be used at the same time.  One program does not affect the other as they are separate systems.  Changing the RealSense Viewer settings, for example, will not affect the ROS setup. 

    You may find though that you cannot access the camera with one of the programs whilst the other is accessing it, because the camera is in a "busy" state.

    If you are only receiving the control_transfer returned error at ROS launch and the warning is not generating continuously then it is not a cause for concern.

    Do you still have the Hardware Notification:RT IC2 Config error if using ROS on its own without the Viewer running, please?

    0
    Comment actions Permalink
  • Howoncheong

    Thanks Marty.
    I don't use them simultaneously.
    I meant that after turn off the roslaunch, the realsense viewer cannot find the camera.
    And I still have the Hardware Notification:RT IC2 Config error whilst I use only ROS launch.

    Thanks :)

    0
    Comment actions Permalink
  • MartyX Grover

    A RealSense support team member provides some advice to try on the RealSense ROS GitHub forum in the link below.

    https://github.com/IntelRealSense/realsense-ros/issues/887#issuecomment-548190289 

    0
    Comment actions Permalink

Please sign in to leave a comment.