L515 example code
Hi,
We have Realsense D415 and have recently bought L515 camera too.
I am currently using the latest version of realsense library (2.35.2).
Using the example code "rs_capture.cpp", I am able to grab data from D415 successfully.
But with L515, I am getting following error.
./rs-capture
22/06 13:43:41,758 ERROR [140049509087040] (types.h:307) Failed to open scan_element /sys/devices/pci0000:00/0000:00:03.0/0000:09:00.0/usb6/6-3/6-3:1.7/0003:8086:0B64.000F/HID-SENSOR-200076.3.auto/iio:device1/scan_elements/in_anglvel_x_en Last Error: Permission denied
22/06 13:43:41,758 ERROR [140049509087040] (backend-hid.cpp:969) Hid device is busy!
RealSense error calling rs2_pipeline_start(pipe:0x2683040):
Failed to open scan_element /sys/devices/pci0000:00/0000:00:03.0/0000:09:00.0/usb6/6-3/6-3:1.7/0003:8086:0B64.000F/HID-SENSOR-200076.3.auto/iio:device1/scan_elements/in_anglvel_x_en Last Error: Permission denied
-
Hi Mshuja Ahmed Technical questions about the L515 are being handled on the RealSense ROS GitHub forum. Could you re-post your question on the GitHub forum please? Thanks!
Please sign in to leave a comment.
Comments
1 comment