RealSense Support

try_wait_for_frames slows down

Comments

3 comments

  • MartyG

    Hi Qi Yao  wait_for_frames is best suited to single camera applications.  For multi camera applications, poll_for_frames should be used, in combination with a 'sleep' instruction to regulate when the CPU is put to sleep to save processing and for how long to sleep.

    In the link below, the RealSense SDK Manager explains the difference between the types of for_frames instructions.

    https://github.com/IntelRealSense/librealsense/issues/2422 

    0
    Comment actions Permalink
  • Qi Yao

    Hi Marty,

      I have read the explanation, but this doesn't seems to address my issue at the core. From my understanding of the thread, the reason to use poll_for_frames is because there is no build in logic to wait for frames from multiple devices. The D415 are hardware synced so my implementation of pulling multiple camera is by using a dedicated std::thread and pull as quickly as possible and each using an separate pipe that is corresponding to a camera. This doesn't create any slow down when I'm simply saving the buffer into disc as images and previewing on monitor, and I was able to use current implementation with 8 cameras with no problem at all. The slow down only happens when I'm start doing 3D reconstructions by having GPU combine all the color and depth into an voxel grid. Just a note, processing power is not the issue here, my CPU is not even 50% utilized and GPU is only about 50% utilized. Also, when using poll_for_frames, since the computer CPU is in charge of timing, how to prevent drifting between CPU and camera clock? As CPU's 33 ms firing and sleeping cycle is not going to be perfectly synced with camera's 33 ms cycle.

    0
    Comment actions Permalink
  • MartyG

    If your GPU is not fully utilised but you need processing acceleration, an option may be to add specialist hardware acceleration to your vision application with an Intel Neural Compute Stick 2, which can plug into a USB port on the computer.  It is available from the official RealSense online store, in a bundle with a camera or on its own.

    https://store.intelrealsense.com/buy-intel-neural-compute-stick-2.html 

    0
    Comment actions Permalink

Please sign in to leave a comment.