[SkeletonTracker] Loading model Exception: cubemos Error
I installed cubemos and try to execute a .exe from a build Unity with a camera D435.
The camera is working.
I can see in the log this error :
"cubemos Error
[SkeletonTracker] Unable to load model from path C:\Users\poc\AppData\Local\Cubemos\SkeletonTracking\models\fp16\skeleton-tracking.cubemos Exception: cubemos Error"
"skeleton-tracking.cubemos" is in the folder and I tried to uninstall and install cubemos again to see if it was not a problem with the file.
I have SDK v2.3.1 and I tried to launch cubemos it works.

The project work on another computer with the same spec.
The project Unity is just the "HelloCubemosScene" that is given with the installation of the SDK.
Where could my problem come from ?
Thank you in advance for your answers
-
Hello Stagiaire I built the same Cubemos example in a new Unity project and had the same problems with finding a model. The 30 day free trial period that I had on the Skeleton Tracking SDK has run out though, so I cannot be sure that this was not blocking the project from running.
I recommend contacting Cubemos, as the Cubemos Skeleton Tracking SDK is their product and not an Intel one.
-
Hi, thank you for your reply MartyG.
I contacted cubemos and my problem is solved.
I post the answer if someone has the same problem later :
"Many thanks for your mail! It can depend on the hardware that you are using. The unity wrapper in the current release tries to use the GPU which is embedded on the CPU. However this does not work, if you have an external GPU.
If you have an external GPU, could you try the previous release?
Please sign in to leave a comment.
Comments
3 comments