RealSense Support

Getting the SR305 to work with the SR300 DCM

Comments

5 comments

  • MartyG

    The RealSense website has a guide to restoring the SR300 compatibility with old programs.  It suggests downloading the DCM installer file (intel_rs_dcm_sr300_3.3.27.5718.exe) with a link in the guide called Download the driver that leads to a download page for the driver, but not running the driver with the normal double-leftclick method after it is downloaded. 

    https://support.intelrealsense.com/hc/en-us/articles/360022951533-Windows-10-Issues-with-Intel-RealSense-Cameras-SR300-and-F200  

     

     

    Instead, go into the Windows Command Prompt and run the file using a special command.

    intel_rs_dcm_sr300_3.3.27.5718.exe --ignore-fw-update --silent --no-progress --acceptlicense=yes

     

    You can find the Command Prompt by going to the text box at the bottom of your Windows screen (next to the button in the corner where you shut down the PC) and typing 'command' into the text box.

    0
    Comment actions Permalink
  • Corvon07

    It starts out where it ask for permission to run the program, but that's as far as it goes The installer don't come up

    0
    Comment actions Permalink
  • MartyG

    Note that it says in the command that it runs silently and does not notify of progress.  Can you now try the SR305 with an SR300 application such as Facerig and see if the camera now works please?

    0
    Comment actions Permalink
  • Corvon07

    Still no luck. Looks like facerig needs the DCM to be running in the background for it to work.

    0
    Comment actions Permalink
  • MartyG

    As far as I know the DCM just acts as a driver and firmware installer.  In 2017 Intel introduced automatic download and install of SR300 drivers in Windows when the camera was plugged into a USB port on an internet connected computer, making the DCM unnecessary except for PCs that did not have internet.

    I knew of a method posted by a RealSense user for restoring the SR300's ability to work with old programs and had been searching for it for you.  I finally managed to locate the link.

    https://support.intelrealsense.com/hc/en-us/community/posts/360038275074-Managed-SR300-to-work-on-latest-Windows-10-18363-535- 

     

    If you are using the free IRFacerig for RealSense, the main version of Facerig can work with ordinary webcams if you need the program and cannot get it working with your SR305, though it is a paid product.

    https://store.steampowered.com/app/274920/FaceRig/

    https://facerig.com

    0
    Comment actions Permalink

Please sign in to leave a comment.