RealSense Support

3D reconstruction/ SFM with a monocular camera and The T265

Comments

3 comments

  • MartyG

    T265 questions are now handled by the RealSense GitHub forum.  you can post your question there by visiting the link below and clicking the 'New Issue' button.

    https://github.com/IntelRealSense/librealsense/issues 

    Having said that, if you are asking whether the T265 can work with a non-RealSense depth camera, the answer should be yes.  Point number 2 of an FAQ for the T265 on its documentation page says about the question of whether it can be used with a depth camera: "Yes, this device can be used with RealSense (and most likely any 3rd-party) depth cameras.  It is passive and comes with an IR-cut filter".

    https://github.com/IntelRealSense/librealsense/blob/master/doc/t265.md#faq 

    I cannot offer guarantees that the T265 will work with a specific non-RealSense model of depth camera though.

    0
    Comment actions Permalink
  • Rakshith Madhavan

    Hello MartyG,
    Thank you for your response. I will pose further queries in the github repo Issues. 
    I was wondering if anyone had done  any work for such a case where a monocular camera + T265 was done. 

    0
    Comment actions Permalink
  • MartyG

    I did a extensive search for examples of the T265 being used with a monocular camera but could not find any.  One approach might be to use a D435 stereo camera instead of the D435i.  The T265 has the same IMU component as the D435i (though processes the IMU data in a different way) and so you only need the T265 for the IMU data and can use the IMU-less D435 model for the depth data.

    There was a video on YouTube where the T265 was being used with the RealSense SR305, which is a depth camera but not stereo like the D435 / D435i (it is Structured Light technology instead).

    https://www.youtube.com/watch?v=k77N50OSuH4 

    0
    Comment actions Permalink

Please sign in to leave a comment.