RealSense Support

Detect and track Ball with D435 in Unity

Comments

5 comments

  • MartyG

    If you want your application to follow only a ball and ignore everything else, object detection and coordinate reading using a Deep Neural Network (DNN) may work well for you.  It can identify an object from an RGB color image and then calculate XYZ coordinates for the currently detected position of that identified object.

    The RealSense SDK has an example DNN program that uses OpenCV and C++.

    https://github.com/IntelRealSense/librealsense/tree/master/wrappers/opencv/dnn 

    You can find specific examples of using a DNN for ball detection by googling for 'dnn ball'.  Here is an example project for ball recognition:

    https://github.com/Isaac25silva/Ball_detect-DNN 

    0
    Comment actions Permalink
  • Sergipanadero

    Thanks you.

    I will start looking at that example and if I find any problem I ask again.
    My greatest fear is the speed of refreshment. I need it to be fast and in the example of that code I see that the refreshment is quite slow.

    0
    Comment actions Permalink
  • MartyG

    If your project budget allows it, you could add an Intel Neural Compute Stick 2 into a USB port alongside your RealSense camera for hardware acceleration of vision computing applications.  The Stick is sold in the official RealSense store, in a bundle with a camera or on its own.

    https://store.intelrealsense.com/buy-intel-neural-compute-stick-2.html 

    Applications created with the RealSense SDK can also have their speed improved by offloading work from the computer's CPU to its graphics GPU.  This can be done by building the SDK with CUDA support if you have an Nvidia GPU, or with an SDK method called GLSL Processing Blocks if you have a non-Nvidia GPU.

    https://github.com/IntelRealSense/librealsense/issues/4905#issuecomment-533854888 

    0
    Comment actions Permalink
  • Sergipanadero

    Thanks you MartyG,
    I undertand that as OpenCV with dnn is made only for c++, python and also javascript. We can't use Unity to detect the ball with the realsense?
    We need to do an application on c++ that detect the ball and pass the data to unity by messages?
    I'm a little los with how to train my own coffemodel dnn to detect a ball.

     

    0
    Comment actions Permalink
  • MartyG

    There is a Unity implementation of OpenCV in the Unity Asset Store, though it is not inexpensive and I could not make guarantees that an OpenCV DNN program would work in it.

    https://assetstore.unity.com/packages/tools/integration/opencv-for-unity-21088 

    Another approach to tracking a specific object with a 400 Series camera is to attach image tags called Aruco markers to the surface of the object so that the camera can detect the tag and capture the object's "pose" (its position and rotation).  It might not be appropriate for a ball used in real play though, as you would need a visible tag on every side of the ball.

    In the early days of RealSense SDK 2.0, a developer created a RealSense Aruco tracker in Unity that used the OpenCV for Unity software mentioned above.

    https://github.com/ajingu/RealSense#aruco 

    0
    Comment actions Permalink

Please sign in to leave a comment.