RealSense Support

Realsense viewer wont open for new D415

Comments

36 comments

  • MartyG

    Your Intel graphics should work fine with the camera.  Do you use Windows 10?  If so, have you downloaded and installled the full 750 mb RealSense SDK please?

    0
    Comment actions Permalink
  • Tom

    Thanks marty,

    yes- windows 10. did you mean the 635mb file?

    Intel.RealSense.SDK-WIN10-2.33.1.1360.exe   635 MB?

    0
    Comment actions Permalink
  • MartyG

    The file size varies depending on the version but yes, that is the full SDK file for the 2.33.1 SDK version.  There is a newer version 2.34.0 (750 mb) that has recently been released though.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.34.0 

    0
    Comment actions Permalink
  • Tom

    Hi,

    Still no luck. I downloaded/installed 2.34.0, clicked the RS desktop icon, nothing. rebooted. nothing

    0
    Comment actions Permalink
  • MartyG

    Does the Depth Quality Tool launch icon work?  They have similar programming, so if there is a problem outside of the Viewer that stops it from launching then it should affect the Depth Quality Tool in the same way.

    Also, does the Viewer launch if you right-click on its launch icon and select the Open menu option?

    0
    Comment actions Permalink
  • Tom
    thanks,
     neither the viewer or the depth tool open at all when i open the menu and try there
    0
    Comment actions Permalink
  • Tom

    my machine is Lenovo ThinkPad X1 Yoga, in case that's helpful

    0
    Comment actions Permalink
  • MartyG

    Thanks for the details.  The most likely explanation is some kind of conflict with the OpenGL graphics support on your device that prevents the Viewer and the Depth Quality Tool from launching.

    Please test the camera with the SDK's Capture tool to see if it launches.  This should be at this drive location:

    C: > Programs and Files (x86) > Intel RealSense SDK 2.0 > Tools > rs-capture.exe

    0
    Comment actions Permalink
  • Tom

    Yes, it has started opened

    0
    Comment actions Permalink
  • Tom

    I get both depth and color images, plus a screen of capture data...

    0
    Comment actions Permalink
  • MartyG

    It does seem likely that the problem is specific to OpenGL graphics support on your computer.  Having said that, the version of the RealSense Viewer that comes with SDK 2.34.0 has been having some problems.  A way to check whether these problems are responsible for your launch issue would be to download SDK 2.33.1's version of the Viewer (the 28.4 mb Viewer file, not the full SDK).

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.33.1 

    0
    Comment actions Permalink
  • Tom

    Thanks. Just tried this and still nothing. should I uninstall anything first?

    0
    Comment actions Permalink
  • MartyG

    Uninstalling the SDK is unlikely to solve the problem, since rs-capture is working: the problem seems specific to the Viewer and Depth Quality Tool.

    There is a program for Windows called OpenGL Extensions Viewer that can be used to test whether OpenGL is working properly on your computer.

    https://www.realtech-vr.com/home/glview 

    0
    Comment actions Permalink
  • Tom

    ok ive run this. how do I see if OPENGL is working as it should?

    0
    Comment actions Permalink
  • Tom

    its Open GL version 4.6

    0
    Comment actions Permalink
  • Tom

    ..updating drivers..

    0
    Comment actions Permalink
  • MartyG

    Its options tabs should have some test modes.

    0
    Comment actions Permalink
  • Tom

    opened extensions 

     

    0
    Comment actions Permalink
  • Tom

    should I be looking for something?

    0
    Comment actions Permalink
  • MartyG

    It is meant to offer a rendering test.  It looks as though the play button for the rendering test does not show on-screen if you are using the program on a small monitor though, unfortunately.

    It sounds as though you have tried updating your graphics drivers and it did not make a difference though.

    0
    Comment actions Permalink
  • Tom

    I ran the rendering test. Not sure how to interpret the results, but all benchmarks where listed as 'OK'

    0
    Comment actions Permalink
  • MartyG

    Okay, thank you very much.

    If the desklop shortcut launch icon does not work, are you able to launch the Viewer directly from the 'Tools' folder using the realsense-viewer file?

    0
    Comment actions Permalink
  • Tom

    Hi Marty,

     No I cant open it from the file

    0
    Comment actions Permalink
  • MartyG

    I located a case where a failure to launch the Viewer in Windows may be caused by a problem with the user documents folder path rather than the graphics drivers.  One of the two users in that discussion also had Intel UHD 620 and experienced failure to launch despite driver updates.

    https://github.com/IntelRealSense/librealsense/issues/4569 

    0
    Comment actions Permalink
  • Tom

    Thanks Marty,

     in C;/User/ there is a DAT File sitting alone titled NTUSER.DAT 3840KB. Is this a realsense file? Last modified yesterday

    0
    Comment actions Permalink
  • MartyG

    No, it's not a RealSense file.  It's a Windows user configuration file and so should be left alone.

    https://www.faqforge.com/windows/windows-10/what-is-the-ntuser-dat-file-in-windows-10/ 

    0
    Comment actions Permalink
  • Tom

    OK thanks,

     So I should create a folder titled Documents in C:/users/Tom and reinstall the SDK?

    0
    Comment actions Permalink
  • MartyG

    The way I read the suggested folder format is that it would look like C:\Users\Tom\Documents

    If you already have the SDK installed then I would recommend just trying to launch the Viewer once the folder structure is created.

    0
    Comment actions Permalink
  • Tom

    SUCCESS!! Both Viewer and depth quality tools now open

    Thanks for all your help Marty. I'll take it from here, t

    0
    Comment actions Permalink
  • MartyG

    Awesome news!  I'm really pleased for you.  Good luck with RealSense!   :)

    1
    Comment actions Permalink

Please sign in to leave a comment.