RealSense Support

D435 Corrupted depth image

Comments

1 comment

  • MartyG

    If a reset corrects the problem then it is likely not a camera calibration problem.  It sounds more like an environmental event such as a flash of light (such as sunlight) causing the IR sensor to become saturated and freeze up.  The depth image is generated from the left and right IR sensors.

    There was a case where this was occurring indoors because sunlight would reflect onto the camera off a glass door in a room when the door opened.  This is part of a much larger discussion in the link below.

    https://github.com/IntelRealSense/librealsense/issues/5209 

    The approach that some users have taken is to program in a hardware_reset() instruction into their application that can reset the camera automatically without human intervention.  They program it to activate on satisfaction of a certain condition.  For example, if a certain percentage of the depth pixels (e.g greater than 50%) have a value of zero (indicating that something has gone wrong with the image) then initiate a camera reset. 

    0
    Comment actions Permalink

Please sign in to leave a comment.