RealSense Support

How to convert units of .ply files to Millimeters in Intel Realsense Viewer

Comments

1 comment

  • MartyG

    Others have encountered this scaling problem in the past.  The scale in the RealSense Viewer has to be set to the same scale as the program that the ply is being imported into.

    Under the 'Controls' section of the Viewer's side-panel options there is a setting called 'Depth Units' whose values are in millimeters (meters / 1000).  Its default value is '0.001' (1 meter), and it can be reduced to a minimum of '0.0001' (0.1 meters) or increased to a maximum of '0.0100' (10 meters).

    0
    Comment actions Permalink

Please sign in to leave a comment.