RealSense Support

D435 Windows 7 32bit

Comments

3 comments

  • MartyG

    The RealSense 400 Series cameras are extremely flexible in regard to hardware requirements.  They should work with any Intel or ARM processor, whatever its capabilities.  There have been a small number of reported cases where they have worked with other processor types such as AMD Threadripper, but no guarantees can be made about processors that are not Intel or ARM.

    If you are only using a single camera then a low-specification, low power computing device should work with it (the RealSense SDK's Windows 7 installation instructions state that multiple cameras are not likely to work with Windows 7 anyway)..

    The installation instructions are here:

    https://github.com/IntelRealSense/librealsense/blob/master/doc/installation_win7.md 

    0
    Comment actions Permalink
  • Prodriguez

    Thank you very much MartyG for you quick and useful response (as usual)

    Best regards

     

    0
    Comment actions Permalink
  • MartyG

    I'm pleased I could be of help.   Good luck with your Windows 7 project!

    0
    Comment actions Permalink

Please sign in to leave a comment.