RealSense Support

passive illumination mode for D435i/L515

Comments

1 comment

  • MartyG

    The RealSense 400 Series cameras can use natural ambient light instead of their built-in IR projector to analyse the depth in the scene.  Unlike many depth cameras, the stronger the light, the better the 400 Series performs.  In a well-lit scene, the IR projector could be turned off.

    The final page (Section 15) of Intel's camera tuning guide offers advice on using the camera in natural light conditions.

    https://www.intelrealsense.com/wp-content/uploads/2019/11/BKMs_Tuning_RealSense_D4xx_Cam.pdf 

    The forthcoming L515 is Lidar depth-sensing technology, rather than the Stereo depth sensing technology used in the 400 Series.   It is best suited for use indoors or in controlled lighting conditions.

    0
    Comment actions Permalink

Please sign in to leave a comment.