RealSense Support

Getting length, width and height of an object

Comments

1 comment

  • MartyG

    The D415 is better for scanning non-moving objects as it has around 2.5x the image quality of D435 (and so less error when measuring from a distance).   It has a smaller field of view size though so it has to be further away from large objects to fit it fully in its view. 

    At the 2m height that you are sensing the box from in your image and the amount of empty space around it, you may be able to have a D415 at the same distance and still fit the box in its view.

    The link below discusses error over distance, which increases linearly as an observed object is further away from the camera.

    https://github.com/IntelRealSense/librealsense/issues/4894 

    For C#, a RealSense user who was also measuring a box from above posted a volume measuring script that may be a good starting point for you.

    https://github.com/IntelRealSense/librealsense/issues/2657 

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.