RealSense Support

How can I get the extrinsic and intrinsic parameter of the T265?

Comments

3 comments

  • MartyG

    T265 extrinsics and intrinsics have been available from the RealSense SDK since version 2.20.0 in April 2019.  You can list them with the rs-enumerate-devices SDK tool, using the instruction rs-enumerate-devices -c

    https://github.com/IntelRealSense/librealsense/issues/3621 

    The source code for the rs-enumerate-devices tool can be found in the link below.

    https://github.com/IntelRealSense/librealsense/tree/master/tools/enumerate-devices 

    If you have Windows and have downloaded and installed the pre-built binary version of the SDK, a pre-built executable version of rs-enumerate-devices can also be found in the following SDK folder:

    C: > Program Files (x86) > Intel RealSense SDK 2.0 > Tools

    0
    Comment actions Permalink
  • Happenzj

    Thanks Marty

     I have got  the extrinsic and intrinsic parameter of the camera!

    0
    Comment actions Permalink
  • MartyG

    You're very welcome.   I'm glad I could help you to get what you needed.   :)

    0
    Comment actions Permalink

Please sign in to leave a comment.