View my account

D435 and T265 for Navigation

Comments

23 comments

  • MartyG

    If the D435 launches before the T265 then it can prevent the T265 from being detected correctly.  A number of people encountered this issue, and it is discussed in the link below.

    https://github.com/IntelRealSense/realsense-ros/issues/774 

    As indicated in the discussion, code was added to the RealSense ROS wrapper to help address the problem.  The wrapper also later added the option to launch devices by USB port ID instead of serial number with the usb_port_id instruction.

    https://github.com/IntelRealSense/realsense-ros#launch-parameters 

    I also recommend using the launch file designed for using the T265 and a depth camera together if you are not launching this way already.

    roslaunch realsense2_camera rs_d400_and_t265.launch

    Regarding the question about the best way to save the 2D occupancy map, I recommend posting a question at the RealSense ROS GitHub forum.  You can do so by visiting the link below and clicking the New Issue button.

    https://github.com/IntelRealSense/realsense-ros/issues 

    As far as I know, the wheel odometry Python sample program that you linked to is the most recent official example and the best solution currently available.  You may also be interested in new wheel odometry calibration information that was recently added to the T265 documentation.

    https://github.com/IntelRealSense/librealsense/blob/master/doc/t265.md#extrinsic-calibration-for-wheeled-odometry-examples 

    The link below provides some good tips on improving accuracy once the T265 is in motion.

    https://github.com/IntelRealSense/librealsense/issues/3970 

    Intel has published an excellent guide to using the T265 and a 400 Series camera together.

    https://dev.intelrealsense.com/docs/depth-and-tracking-cameras-alignment 

    0
    Comment actions Permalink
  • Vikranj

    Thanks for the reply!

    Are the code samples for demo in the video (https://www.youtube.com/watch?v=62vm0_RZ1nU&feature=youtu.be&t=1036) released?

     

    0
    Comment actions Permalink
  • MartyG

    I hope that the link below will be helpful to you. 

    https://github.com/IntelRealSense/librealsense/blob/master/doc/t265.md#examples-and-tools 

    0
    Comment actions Permalink
  • Andre

    could you make launch file for 265/d400/l515, please? to run all three of them?

    do you provide any support for running librealsense ROS wrapper on Jetson? Within docker container? Shall I create a separate post for the purpose?

    reference https://community.intel.com/t5/Graphics/librealsense-support-on-nvidia-Jetson-hardware-ros-wrapper-won-t/td-p/1192358

    "ROS2 wrapper works; but ROS1 wrapper would thhrow many mwessages after starting the node:"

    INFO] [1591601602.923007659]: RealSense Node Is Up! 08/06 00:33:22,965 ERROR [546442297728] (synthetic-stream.cpp:48) Exception was thrown during user processing callback! 08/06 00:33:22,974 WARNING [547130171776] (messenger-libusb.cpp:42) control_transfer returned error, index: 768, error: No data available, number: 61 08/06 00:33:22,994 ERROR [546442297728] (synthetic-stream.cpp:48) Exception was thrown during user processing callback! 08/06 00:33:23,026 ERROR [546442297728] (synthetic-stream.cpp:48) Exception was thrown during user processing callback! 08/06 00:33:23,035 WARNING [547130171776] (messenger-libusb.cpp:42) control_transfer returned error, index: 768, error: No data available, number: 61 08/06 00:33:23,059 ERROR [546442297728] (synthetic-stream.cpp:48) Exception was thrown during user processing callback!

     

     

    reference https://forums.developer.nvidia.com/t/realsensed400-camera-can-not-work-on-jetson-xavier-nx/125138/24

    0
    Comment actions Permalink
  • MartyG

    Hi Andre  Can you re-post your message on the RealSense ROS GitHub forum please, as cases involving the T265 or L515 are not handled on this forum.  You can do so by visiting the link below and clicking on the New Issue button.   Thanks!

    https://github.com/IntelRealSense/realsense-ros/issues 

    0
    Comment actions Permalink
  • Andre

    Hi MartyX Grover, Thank you for following up.

    Which issues are covered at this forum? D435? D435i? they throw the message listed above. t265 seems working. l515 seems to throw the same messages as d series. I will try to post to github, However, in the past, I believe I posted to tere and haven't got any response.

    as you can see no one responded there https://github.com/IntelRealSense/realsense-ros/issues/1287

    we got a bunch of librealsenses bought including t265, d435, d435i, l515, and none of them but for t265 work from nvidia Jetson Xavier. Is it likely that Intel will help with getting them running with ros wrapper via the github? at all?

    0
    Comment actions Permalink
  • MartyG

    All camera issues not related to T265 and L515 can be handled on this forum.  This includes all 400 Series cameras and SR300 / SR305.

    I am on both this forum and the two GitHubs (the main one and the ROS one).  Someone else is responsible for T265 and L515 cases though, which is why I was not able to take up your linked ROS GitHub case because it mentioned L515 and T265.  The developer of the RealSense ROS wrapper is based at the ROS GitHub though.

    I recommend closing the linked case and re-posting it with the middle comment about L515 / T265 left out, so that I can take on that case tomorrow if it only mentions D435 / D435i.  Please post the L515 issue as a separate case so that the person who handles L515 can give it their attention.  Thanks for your patience!

    0
    Comment actions Permalink
  • Andre

    thank you for the update;

    I dissected everything about l515 and t265 from the github issue.

    Will it work for you?

    R u aware if there are launchfiles that will run all three devices?

    0
    Comment actions Permalink
  • MartyG

    Thanks very much, your edit was a good approach.  I will make a note to look at it tomorrow (I am off-duty now).  

    There is a tutorial for using two 400 Series cameras together here:

    https://www.intelrealsense.com/how-to-multiple-camera-setup-with-ros/ 

    You can also launch more than one camera with rs_multiple_devices.launch

    https://github.com/IntelRealSense/realsense-ros#work-with-multiple-cameras 

    A 400 Series and T265 can also launch together with roslaunch realsense2_camera rs_d400_and_t265.launch

    T265 on its own can be launched with rs_t265.launch

    https://github.com/IntelRealSense/realsense-ros#using-t265 

    It looks as though L515 can use roslaunch realsense2_camera rs_camera.launch filters:=pointcloud

    https://github.com/IntelRealSense/realsense-ros/issues/1246 

     

    0
    Comment actions Permalink
  • Andre

    thank you for the update!

    0
    Comment actions Permalink
  • MartyG

    A RealSense support team member has now taken on your ROS GitHub cases.

    0
    Comment actions Permalink
  • Andre

    there are issues implementing ros2-foxy-librealsense2

    instruction https://github.com/intel/ros2_intel_realsense/tree/refactor#install-ros2_intel_realsense-from-source won't work

    command sudo apt-get install ros-foxy-librealsense2 wouldn't find apt package 

    building from sources would return multiple errors, e.g.

    CMake Error at /opt/ros/foxy/share/std_msgs/cmake/ament_cmake_export_dependencies-extras.cmake:43 (get_target_property):
    get_target_property called with incorrect number of arguments
    Call Stack (most recent call first):
    /opt/ros/foxy/share/std_msgs/cmake/std_msgsConfig.cmake:41 (include)
    CMakeLists.txt:20 (find_package)

    0
    Comment actions Permalink
  • MartyG

    Hi Andre  I cannot provide any further information here as this particular case is being handled by another RealSense support team member on the ROS GitHub now.  

    0
    Comment actions Permalink
  • Andre

    on the ROS github where?

    https://github.com/IntelRealSense/realsense-ros/issues/1287 ??

    at some other thread?

    Thanks

    0
    Comment actions Permalink
  • MartyG

    Yes on #1287 where you posted the Foxy question a little earlier.  The RealSense team member RealSenseSupport is handling your case.

    https://github.com/IntelRealSense/realsense-ros/issues/1287#issuecomment-660253774 

    0
    Comment actions Permalink
  • Andre

    can you help out with running calibration on d435? d435i? self calibration? https://www.google.com/amp/s/www.intelrealsense.com/self-calibration-for-depth-cameras/amp/

    dynamic calibration?

    for the latter I can not find packages in the added aws librealsense repository; for arm architecture

    0
    Comment actions Permalink
  • MartyG

    Hi Andre  I have responded to your self calibration question on the GitHub.

    https://github.com/IntelRealSense/realsense-ros/issues/1287#issuecomment-661858975 

    The top of page 16 of the user guide for the Dynamic Calibrator explains how you can install through a local file as well as the AWS method described on page 15.

    https://www.intel.com/content/dam/support/us/en/documents/emerging-technologies/intel-realsense-technology/RealSense_D400_Dyn_Calib_User_Guide.pdf 

     

    0
    Comment actions Permalink
  • Andre

    Thank you for you rresponse!

    At the moment I am trying to find out how to run remotely realsense viewer in oder to approach self-calibration; It wouldn't run over X forward.

    Regarding the dynamic calibration I was looking where to download the deb files. May be there is some url where they can be downloaded? specifically for arm64?

    0
    Comment actions Permalink
  • MartyG

    My interpretation of the instructions for the 2.11.0.0 version (July 2020) of the Dynamic Calibrator tool is that it needs to be installed using the Linux installation method for Ubuntu 16.04 / 18.04   This would suggest that the AWS method needs to be used, since the local file is described as being in AMD64 format (i.e not Arm architecture).

     

     

    Did you follow the instructions for Linux installation from page 14 of the guide please, completing the prerequisites before trying to access the AWS address on page 15?

    0
    Comment actions Permalink
  • Andre

    Yes, thank you for looking into the issue; I have read the instruction; However, after executing all steps I can not find the arm64 package in the aws repository; the same time at x86_64 device the file gets from the added aws repository;

     

    0
    Comment actions Permalink
  • MartyG

    I checked the instructions very carefully but there is no further guidance about Arm.  Can you ask about it on the main GitHub please by creating a case there?  Thanks!

    https://github.com/IntelRealSense/librealsense/issues 

    0
    Comment actions Permalink
  • Andre

    Thank you for following up!

    I am being asked if it is possible to implement finger/gesture/hand tracker like illustrated in the article https://www.intelrealsense.com/hand-tracking-overview/

    with use of d400 devices.

    Could you share any insights regarding implementation on d400 on linux something like is described into the article, please?

    0
    Comment actions Permalink
  • MartyG

    Finger and hand tracking is not strongly supported on the 400 Series cameras by existing programs.  Nuitrack SDK can do hand gesture recognition, and they also have a new Nuitrack AI product in development that can do finger tracking.

    https://nuitrack.com/ 

    Intel published a seminar about body joint tracking for RealSense.  It requires you to use multiple cameras to train a data-set though before that data can be used for tracking with a single camera.

    https://www.youtube.com/watch?v=VSHDyUXSNqY 

    0
    Comment actions Permalink

Please sign in to leave a comment.