View my account

Interfacing D435i with Raspberry Pi Zero W

Comments

1 comment

  • MartyG

    The 400 Series cameras can be used with boards that have an OTG port (such as the original Up Board) via an adaptor,

    Until recently, it was hard to get the D435i to work with Raspbian Buster.  SDK version 2.30.0 added a fix for the build process though, so it should be okay now.

    Before Raspberry Pi 4, the USB ports on Pi boards were USB 2.0.  So USB 2.0 would provide some operational limitations for the camera, as it needs a USB 3 connection to access its full range of features and capabilities.

    https://www.intelrealsense.com/usb2-support-for-intel-realsense-technology/ 

    0
    Comment actions Permalink

Please sign in to leave a comment.