RealSense Support

D400 Series Calibration

Comments

9 comments

  • MartyG

    Doing an OEM calibration is a good idea for manufacturers integrating the camera into their products, as the act of handling the modules can cause the imagers to require recalibration if the module is flexed during installation.  It is up to the manufacturer whether they take this step.

    If it were an external USB camera, a simple non-OEM calibration of the extrinsics alone with the standard Dynamic Calibrator program would likely be sufficient to correct miscalibration caused by the camera experiencing a physical stress or shock.  In the case of an integrated tablet camera, following the manufacturer advice is recommended.

     Information about on-chip calibration support is in the link below.  Documentation notes (the November 2019 Specification Update)  indicate that alpha support for self calibration and tare calibration was added in firmware 5.11.15.0 and requires at least SDK version 2.29.0.

    https://github.com/IntelRealSense/librealsense/pull/4658 

    0
    Comment actions Permalink
  • Daniel

    Thanks for the link.

    So reading the documentation notes, it seems that both this on-chip calibration and the dynamic calibration affects only the extrinsic parameters of this stereo camera (how the two cameras are positioned relatively). Can we assume the intrinsic parameters in the module are correct and stays correct when the manufacturer receives the modules and installs them?

    The OEM calibration I was referring to is https://store.intelrealsense.com/buy-intel-realsense-d400-cameras-calibration-target.html . Is this the only tool that can do intrinsic calibrations?

     

     

    0
    Comment actions Permalink
  • MartyG

    In 99% of cases, intrinsic calibration by the end-user is not necessary as it is calibration of the extrinsics that have the most effect on image quality and there is no particular disadvantage from being unable to perform intrinsic calibration.  For detailed advice on intrinsic calibration, the RealSense GitHub will be the best place to ask.

    If the OEM calibrator software is unavailable to you, then you could look at Intel's white paper for developing your own custom calibration solution with the custom calibrator API.

    https://www.intel.co.uk/content/www/uk/en/support/articles/000026725/emerging-technologies/intel-realsense-technology.html 

    If you would prefer the existing OEM calibrator software but do not want to purchase the OEM board in the store in order to get it, the only possible way that I know of to get the software on its own is if you have an NDA agreement with Intel.

     

     

    0
    Comment actions Permalink
  • Daniel

    Thanks Marty. You've been a great help!

    0
    Comment actions Permalink
  • Brice Miramont

    Hi MartyG, is it stil possible to have  an NDA agreement with Intel to get the oem calibration software as I need it to calibrate the camera for underwater use in an integrated device ?

    Maybe a used oem kit can be sold as it seems out of stock at the moment.

    thank you,

    Brice

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Brice Miramont  You may not need the OEM calibration software for calibrating for underwater, as there is an extensive discussion on the subject at the link below.

    https://github.com/IntelRealSense/realsense-ros/issues/1723

    A RealSense team member (agrunnet) provided very detailed technical information about underwater calibration at the link below - please read downwards from the point of the discussion that I have linked to.

    https://github.com/IntelRealSense/realsense-ros/issues/1723#issuecomment-808406783

     

    Because the above conversation is so long, please look out for a Load More link to un-hide a substantial amount of the discussion, which also contains details of a custom underwater housing for the camera.

     

     

    Further discussion about underwater calibration can be found here:

    https://github.com/IntelRealSense/librealsense/issues/7966

     

    In regard to applying for an NDA, I would recommend confirming whether or not the information in the above links can provide a solution for you before pursuing NDA application.  If you decide that you want to proceed with application then I can pass your contact details to the appropriate RealSense team member.

    0
    Comment actions Permalink
  • Brice Miramont

    Thank you Marty, agrunnet did succeed in calibrating the camera underwater with the help of the oem calibration toolkit. So my question is, how can I get one and at what cost ? If the hardware is not available, maybe I can make one with the schematics and in that case I'll need the software part from Intel.

     

    thank you

    Brice

    0
    Comment actions Permalink
  • MartyX Grover

    I once asked agrunnet if a home-made version of the large OEM target board could be printed on paper and was told that it would not work, as the target board is made from a special material.

     

    agrunnet did state in the underwater calibration discussion though that Intel were able to test underwater calibration with a smaller board that they made and used in a large fish tank (agrunnet did add to use the OEM board if calibrating in a pool-sized environment).

    https://github.com/IntelRealSense/realsense-ros/issues/1723#issuecomment-834677375

    This suggests that the ordinary small official calibration print target for a single camera that is printed off and mounted on a surface such as a wall might have been used with the fish tank (the OEM board is large sized to support calibration of multiple cameras).

    https://www.intel.com/content/dam/support/us/en/documents/emerging-technologies/intel-realsense-technology/print-target-fixed-width.pdf

     

    In regard to obtaining the OEM board, it does typically come back into stock after being out of stock (I observed that it was in stock last week before it went out of stock).  You can subscribe in the store listing for the board to be notified when it is back in stock.  The official RealSense Store is the only retailer that stocks the board.

    In regard to obtaining the OEM calibration software without the board, my understanding is that one can request it from their 'local Intel representative' (which is typically an NDA-level support request).

     

    Since the On-Chip calibration can calibrate both intrinsics and extrinsics (though in separate calibration actions rather than in the same calibration session), it may be worth testing whether an On-Chip calibration can provide the desired results.

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Brice Miramont  The $1500 USD OEM calibration target board has just come back into stock in the RealSense Store today.

    https://store.intelrealsense.com/buy-intel-realsense-d400-cameras-calibration-target.html

    0
    Comment actions Permalink

Please sign in to leave a comment.