RealSense Support

T265 vs T261 specifications

Comments

1 comment

  • MartyG

    The data sheet document for T261 and T265 can be found in the link below.

    https://dev.intelrealsense.com/docs/tracking-camera-t265-datasheet 

    The small difference between T261 and T265 is that the T265 adds an 'interposer card' to allow USB connection.  The data sheet says this:

    "The T265 and T261 have one main board which includes all components on a single board.  T265 comprises a T261 module, an interposer card with a USB connector and a peripheral envelope.  The T261 module requires an external interposer card to allow USB connection, in case it is used outside the T265 peripheral". 

    0
    Comment actions Permalink

Please sign in to leave a comment.