Window realsense viewer can not see connected D415
Hello,
I have some issue with opening the D415 with the intel RealSense viewer. But the device was detected in the device manager.
I can see both RealSense 415 Depth and 415 RGB under the imaging devices. But when i run the RealSense viewer or the example hello-realsense, i got the no connected device error. I try to update the firmware to 5.11.15.0 but still no luck with this problem. Can someone help?
Thank you
Please sign in to leave a comment.
Comments
1 comment