RealSense Support

D435 Linux Driver Message Issues

Comments

2 comments

  • Prodriguez

    Update

    SDK: 2.28.0

    Firmware: 5.11.11.100

    0
    Comment actions Permalink
  • MartyG

    A number of other users have experienced this error.  My research indicates that the RealSense team members took a good look at it over these various cases but a single definitive solution did not emerge.  The two main recommendations were to try a kernel upgrade, or use a mains-powered USB hub to help ensure that the camera is not being forcibly disconnected.

    I note that you are using Kernel 4.4, which is the absolute minimum kernel for RealSense SDK 2.0.  Would it be possible to update your project to a more recent kernel, please?

    0
    Comment actions Permalink

Please sign in to leave a comment.