RealSense Support

Construct Frameset Object

Comments

3 comments

  • MartyG

    When capture is activated, if you have auto-exposure enabled then the first several frames are spent settling down the auto-exposure values.  You can either disable auto-exposure and use your own exposure values, or use code to tell the camera to skip the first frames by using a 'for' instruction to wait until there is a complete frameset available.

    https://github.com/IntelRealSense/librealsense/issues/2269#issuecomment-414211209 

    0
    Comment actions Permalink
  • Asfrga

    Hi everyone,

    I am also having this kind of problem. The solution provided by MartyG was not very helpful (rs2::software_sensor does not support auto exposure as an option), so I wonder if anyone can provide a better answer.

    Have you found a valid solution to this problem, Frank?

    I also wrote a program that is based on the software_device example mentioned by Frank (https://github.com/IntelRealSense/librealsense/tree/master/examples/software-device), and my program's structure is very similar to the main function of that example. What I am trying to do is read two images (a depth image encoded as Z16 and a color image encoded as BGR8) from the file system, feed them into their respective sensors, then call sync.wait_for_frames(). What perplexes me is that no matter how many loops I run the frameset I received always only contain 1 frame, and that is the depth frame. The color frame just would not show up. Here is my code:

    #include <iostream>
    #include <opencv2/opencv.hpp>
    #include <librealsense2/rs.hpp>
    #include <librealsense2/hpp/rs_internal.hpp>

    double W = 640;
    double H = 480;


    int main() {

    rs2::software_device dev;

    auto depth_sensor = dev.add_sensor("Depth");
    auto color_sensor = dev.add_sensor("Color");

    rs2_intrinsics depth_intrinsics{W, H, W / 2, H / 2, 383.859, 383.859, RS2_DISTORTION_BROWN_CONRADY,
    {0, 0, 0, 0, 0}};
    rs2_intrinsics color_intrinsics{W, H, W / 2, H / 2, 618.212, 618.463, RS2_DISTORTION_INVERSE_BROWN_CONRADY,
    {0, 0, 0, 0, 0}};

    auto depth_stream = depth_sensor.add_video_stream(
    {RS2_STREAM_DEPTH, 0, 0, W, H, 60, 2, RS2_FORMAT_Z16, depth_intrinsics});
    auto color_stream = color_sensor.add_video_stream(
    {RS2_STREAM_COLOR, 0, 1, W, H, 60, 3, RS2_FORMAT_BGR8, color_intrinsics});

    dev.create_matcher(RS2_MATCHER_DEFAULT);
    rs2::syncer sync;

    depth_sensor.open(depth_stream);
    color_sensor.open(color_stream);

    depth_sensor.start(sync);
    color_sensor.start(sync);

    depth_stream.register_extrinsics_to(color_stream, {{1, 0, 0, 0, 1, 0, 0, 0, 1},
    {0, 0, 0}});

    rs2::frameset fs;

    cv::Mat color_image;
    cv::Mat depth_image;

    //stream in the images
    for (int idx = 0; idx < 120; ++idx) {
    color_image = cv::imread("/home/username/Desktop/images/color.jpg", cv::IMREAD_COLOR);
    depth_image = cv::imread("/home/username/Desktop/images/depth.png", cv::IMREAD_UNCHANGED);

    color_sensor.on_video_frame({(void*) color_image.data, // Frame pixels from capture API
    [](void*) {}, // Custom deleter (if required)
    3 * 640, 3, // Stride and Bytes-per-pixel
    (double) (idx) / 60, RS2_TIMESTAMP_DOMAIN_COUNT,
    idx, // Timestamp, Frame# for potential sync services
    color_stream});
    depth_sensor.on_video_frame({(void*) depth_image.data, // Frame pixels from capture API
    [](void*) {}, // Custom deleter (if required)
    2 * 640, 2, // Stride and Bytes-per-pixel
    (double) (idx) / 60, RS2_TIMESTAMP_DOMAIN_COUNT,
    idx, // Timestamp, Frame# for potential sync services
    depth_stream});

    fs = sync.wait_for_frames();
    }

    return 0;
    }

    Can anyone PLEASE give me some explanation? 

    1
    Comment actions Permalink
  • Nicholasmcdonald40

    Hi everybody,

    This problem still persists in 2021, but I can propose a simple workaround.

    I am also trying to load frames (rgb + depth) from disk and then process them using the standard pipeline by creating frames in a software device. Sadly, the rs-software-device example is not fully functional and fails because the syncer fails to consistently extract the constructed frames.

    I do this particularly because I want to do expensive processing after recording at a separate time and am loading frames from raw byte data.

    The syncer likes to throw a tantrum particularly when the simulated timestamps don't match the FPS of the software sensor. @Asfrga this is a problem in the code you posted. That's why the example multiplies `ind` with 16, which is roughly 1000/60 (unit milliseconds).

    I am not sure under the hood what is preventing the syncer from extracting the frames correctly, I think it has to do with timestamps.

    Here is my original implementation:

    #include <librealsense2/rs.hpp>
    #include <librealsense2/hpp/rs_internal.hpp>
    #include <iostream>
    #include <vector>
    #include <csignal>
    #include <unistd.h>

    struct synthframe{
    int W, H, B;
    std::vector<uint8_t> dat;
    };

    const int CW = 960; //Color Frame
    const int CH = 540;
    const int CB = 4;

    const int DW = 640; //Depth Frame
    const int DH = 480;
    const int DB = 2;

    const rs2_intrinsics intrDepth = { DW, DH,
    324.83203125, 254.3828125,
    456.63671875 , 457.02734375 ,
    RS2_DISTORTION_NONE ,
    { 0,0,0,0,0 } };

    const rs2_intrinsics intrColor = { CW, CH,
    488.421417236328, 268.80029296875,
    673.101379394531, 673.328247070312,
    RS2_DISTORTION_INVERSE_BROWN_CONRADY ,
    { 0.142735555768013, -0.466687560081482, -0.000759649323299527, 0.000336397089995444, 0.420803397893906 } };

    synthframe cframe; //Color-Frame
    synthframe dframe; //Depth-Frame

    synthframe& getColor(){
    //...
    return cframe;
    }

    synthframe& getDepth(){
    //...
    return dframe;
    }

    bool isalive = true;
    void sighandler(int signal){
    isalive = false;
    }

    int main(int argc, char * argv[]) try {

    signal(SIGINT, &sighandler);

    rs2::software_device dev; // Create software-only device
    dev.create_matcher(RS2_MATCHER_DEFAULT);

    auto depth_sensor = dev.add_sensor("Depth"); // Define single sensor
    auto color_sensor = dev.add_sensor("Color"); // Define single sensor

    auto depth_stream = depth_sensor.add_video_stream({RS2_STREAM_DEPTH, 0, 0,
    DW, DH, 100, DB, RS2_FORMAT_Z16, intrDepth });

    depth_sensor.add_read_only_option(RS2_OPTION_DEPTH_UNITS, 0.00025f);

    auto color_stream = color_sensor.add_video_stream({RS2_STREAM_COLOR, 1, 1,
    CW, CH, 100, CB, RS2_FORMAT_RGBA8, intrColor });

    dev.create_matcher(RS2_MATCHER_COUNT);

    color_stream.register_extrinsics_to(depth_stream, {
    { 0.999966, -0.00700524, 0.00429877,
    0.00689519, 0.999661, 0.0251015,
    -0.00447315, -0.025071, 0.999676 },
    {-0.000823423033580184, -0.0139116607606411, 0.00651831179857254 } });

    depth_stream.register_extrinsics_to(color_stream, {
    { 0.999966 , 0.00689519 , -0.00447315,
    -0.00700524 , 0.999661 , -0.025071,
    0.00429877 , 0.0251015 , 0.999676 },
    {0.000697920040693134, 0.0137490043416619, -0.00686865951865911 } });

    depth_sensor.open(depth_stream);
    color_sensor.open(color_stream);

    int ind = 0;

    rs2::syncer sync(2);
    color_sensor.start(sync);
    depth_sensor.start(sync);

    cframe = getColor();
    dframe = getDepth();

    while(isalive){

    color_sensor.on_video_frame({ cframe.dat.data(), // Frame pixels from capture API
    [](void*) {cframe.dat.clear();}, // Custom deleter (if required)
    CW*CB, CB, // Stride and Bytes-per-pixel
    (double)ind*10.0, RS2_TIMESTAMP_DOMAIN_HARDWARE_CLOCK, ind,
    color_stream });

    depth_sensor.on_video_frame({ dframe.dat.data(), // Frame pixels from capture API
    [](void*) {dframe.dat.clear();}, // Custom deleter (if required)
    DW*DB, DB, // Stride and Bytes-per-pixel
    (double)ind*10.0, RS2_TIMESTAMP_DOMAIN_HARDWARE_CLOCK, ind,
    depth_stream });

    usleep(100000); //!!!!!!!!

    ind++;

    rs2::frameset fset;
    try{
    fset = sync.wait_for_frames();
    }
    catch(rs2::error e){
    std::cout<<e.what()<<std::endl;
    }

    std::cout<<"Found "<<fset.size()<<" frames"<<std::endl;
    if(fset.size() == 1){
    std::cout<<"Only Found 1 Frame "<<fset[0].get_profile().stream_type()<<std::endl;
    continue;
    }
    else{
    cframe = getColor();
    dframe = getDepth();
    }

    }

    return EXIT_SUCCESS;

    }
    catch (const rs2::error & e){
    std::cerr << "RealSense error calling " << e.get_failed_function() << "(" << e.get_failed_args() << "):\n " << e.what() << std::endl;
    return EXIT_FAILURE;
    }
    catch (const std::exception& e){
    std::cerr << e.what() << std::endl;
    return EXIT_FAILURE;
    }

    Note that adding usleep(1E5) or processing the frames makes the syncer fail.

    Solution:

    Don't use the syncer. Use a frame queue with a custom bundler as a processing block. Replace this:

    rs2::syncer sync(2);
    color_sensor.start(sync);
    depth_sensor.start(sync);

    with this:

     
    //Prepare frame-set getter (the frame queue!)
    rs2::frame_queue q(2);
    std::vector<rs2::frame> bundle;

    rs2::processing_block bundler([&](rs2::frame f, rs2::frame_source& src) {
    bundle.push_back(f); //add frame to vector
    if (bundle.size() == 2){ //or however many when full
    auto fs = src.allocate_composite_frame(bundle);
    src.frame_ready(fs);
    bundle.clear();
    }
    });
    bundler.start(q); //when enough frames are loaded, the queue is ready

    depth_sensor.start([&](rs2::frame f){
    bundler.invoke(f); //add frame to bundler
    });
    color_sensor.start([&](rs2::frame f){
    bundler.invoke(f);
    });

    Then it stops caring about the timestamp syncing and processing time and just constructs the frameset for you so you can use them.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.