RealSense Support

Frames didn't arrives & USB SCP overflow & REC overflow

Comments

1 comment

  • MartyG

    The problem may be with the 2m USB cables.  Because RealSense cameras can transmit a large amount of data through the USB cable at higher resolutions / FPS, cables longer than the short official ones that are supplied with the camera may have degraded performance or not work at all if the cables are not high-quality premium grade ones.

    Newnex are a supplier of industrial-grade cables proven to work with 400 Series cameras (which use a USB-C, or A to C cable).

    https://www.newnex.com/realsense-3d-camera-connectivity.php 

    0
    Comment actions Permalink

Please sign in to leave a comment.