RealSense Support

Nuitrack Support for Raspberry Pi 3 and Tinkerboard Added

Comments

15 comments

  • Gbenel

    Yes, but as I learned the hard way, nuitrack does not work with realsense on the raspberry pi (nuitrack does not support)

    0
    Comment actions Permalink
  • MartyG

    If you are using a Pi that is not Pi 4 and so have a USB 2.0 connection, Nuitrack has advice about what changes to do in order to use Nuitrack with RealSense and USB 2.0.  I have pasted it below.

    **************

    You can connect RealSense via USB 2.0, but in this case you have to set lower resolution for a depth map.  To do this, open nuitrack.config (%NUITRACK_HOME%/data), find the section "Realsense2Module" and add the following lines to "Realsense2Module.Depth":

    "RawWidth": 640,
    "RawHeight": 480,

    0
    Comment actions Permalink
  • Gbenel

    Ok, I'm using a pi4. It does have a couple USB 2 ports, may be worth trying. I imagine will be very slow though.
    Interesting, when I contacted nuitrack they told me essentially no way to make realsense work with any pi.

    0
    Comment actions Permalink
  • Gbenel

    I have posenet running very well on my rpi4 with a coral edge device, but without using depth data to find skeletons, it struggles for me when two people are near one another. Was hoping nuitrack may perform better as it uses depth data in establishing identifications.

    0
    Comment actions Permalink
  • MartyG

    Another skeletal tracking solution for the RealSense D415, RealSense D435 and FRAMOS D435e cameras was highlighted by Intel during January's CES electronics show.  It's called Cubemos, and will also work with the forthcoming new RealSense L515 lidar-based depth camera.

    https://www.cubemos.com/skeleton-tracking-sdk/ 

    Click on the 'Download SDK' button on the above link to go to a download page that has a link to the PDF user manual for Cubemos.

    Here is a video of it running with the L515:

    https://www.youtube.com/watch?v=PTMo4Dvya1Y&feature=emb_logo 

    0
    Comment actions Permalink
  • Gbenel

    Yes, I have talked with them. Unfortunately they do not support the Jetson platform or raspberry pi platform.

    0
    Comment actions Permalink
  • MartyG

    I did further research on the subject of finding skeletal tracking solutions for RealSense cameras that might work with a Pi, but the possibilities seem to be slim.  Intel did a seminar a while ago on advanced body tracking that is available on YouTube, though it typically requires multiple cameras to generate a data-set for the tracking before it can be used with a single camera.

    https://www.youtube.com/watch?v=VSHDyUXSNqY

    0
    Comment actions Permalink
  • Gbenel

    Posenet works great (with an edge device) but when you have multiple people in the frame relatively close together sometimes things run amok and depth data (in finding skeletons) would be useful (it is easy to get depth data after the fact)

    0
    Comment actions Permalink
  • MartyG

    You can get a basic distance measurement on a person using object recognition with a Deep Neural Network (DNN).  It ought to be able to discern between two different people.  I have seen DNN example programs that can detect more than one person separately.  Here's an example of a program detecting the difference between an object and a human ("Person"):

    https://github.com/twMr7/rscvdnn

    Here is a multi-person example:

    https://github.com/apoorvavinod/Real_time_Object_detection_and_tracking

    0
    Comment actions Permalink
  • Gbenel

    You can see even in their examples on the readme on github that the same person has their id switched while tracking

    0
    Comment actions Permalink
  • MartyG

    Another option for skeletal tracking you could investigate is OpenPose

    https://github.com/stevenjj/openpose_ros 

    0
    Comment actions Permalink
  • Gbenel

    Yes, but again, I don’t think openpose uses depth info to find skeletons thus I don’t think it would be any better than posenet (which is optimized for edge devices and works great in 2d)

    0
    Comment actions Permalink
  • MartyG

    I did further investigation but could not find a solution that would clearly work with Raspberry Pi.  The last resort may be to find out what board will work with existing skeleton tracking solutions and change to that.  I wish you the best of luck.   Sorry I couldn't be of more help.

    0
    Comment actions Permalink
  • Gbenel

    A Nuc would do it but it has a large power requirement - I am working on a wearable device and it would be hard to carry around such a heavy battery

    0
    Comment actions Permalink
  • MartyG

    A more compact alternative to a NUC is the Intel Compute Stick pocket-sized PC.

    https://www.intel.co.uk/content/www/uk/en/products/boards-kits/compute-stick.html 

    0
    Comment actions Permalink

Please sign in to leave a comment.