View my account

R200 no mention on the site? How do we start developing for it?

Comments

1 comment

  • MartyG

    The R200 is a retired product and the RealSense SDK 2.0 software does not support it, unfortunately.  There are two SDKs that support the R200:

    RealSense SDK '2016 R2' for Windows

    This is a 1.8 gb download that can be launched in your browser by left-clicking on the link below.  This is the easiest to use SDK for users new to RealSense.  Please bear in mind that the download may be slow, so give it some time if it looks as though the download counter is not moving.

    http://registrationcenter-download.intel.com/akdlm/irc_nas/vcp/9078/intel_rs_sdk_offline_package_10.0.26.0396.exe 

    Legacy Librealsense

    This is the predecessor of the current RealSense SDK 2.0, and the choice to use if your OS is Linux or Mac.  It also works with Windows.  It is more complex to learn than the '2016 R2' SDK but has a similar language to SDK 2.0, so would make it easier to upgrade to a newer camera later.

    https://github.com/IntelRealSense/librealsense/tree/v1.12.1 

    0
    Comment actions Permalink

Please sign in to leave a comment.