Power Saving with D435
Is there a way to make the D435 camera and processor only run when needed/triggered?
-
The 400 Series cameras are only capturing when the 'pipeline' has been started. So if you stop the pipeline when not capturing then you can have the camera on standby. The 400 Series is more power efficient than its predecessors so this should not use too much power. Page 30 of the data sheet document lists the minimum power draw of the Vision Processor D4's components.
Please sign in to leave a comment.
Comments
2 comments