RealSense Support

D435 external temperature

Comments

3 comments

  • MartyG

    RealSense cameras are regularly tested  by Intel with long running, and can run indefinitely as long as they remain within recommended operating tolerances of 35 degrees C.  You can check in the RealSense Viewer's side-panel options what the current internal temperature of the camera is.

    The fast rate of heating sounds abnormal.  Sometimes a fault in a computer's USB port will cause devices attached to it to heat up rapidly.  Do you have another USB device other than a camera that you can plug in to test whether this is the case with the port?  

    0
    Comment actions Permalink
  • Lab

    Hi Marty, the customer support just contacted me.
    Thank you

    0
    Comment actions Permalink
  • MartyG

    Thanks for the update!

    0
    Comment actions Permalink

Please sign in to leave a comment.