RealSense Support

D455 Poor depth quality

Comments

3 comments

  • MartyG

    Hi Liam Neric  The problem with the D455 depth image seems to occur with the depth nearest to the camera.  the D435 has a minimum depth sensing distance of around 0.15 meters, whilst D455's minimum is around 0.5 meters.

     

    I would therefore recommend excluding the possibility that the broken depth areas on D455 represent distance values that are nearer to the camera than 0.5 meters.  You could test this using a setting called Disparity Shift that reduces the minimum distance of the camera and enables depth that is closer to it to be successfully included on the depth image.

     

    1.  Go to the Advanced Controls section of the RealSense Viewer's options side panel and expand open its options.  

    2.  Expand open the Depth Table settings under Advanced Controls.

    3.  Find the Disparity Shift option, which has a value of 0' by default and change it to '200'.

     

    Are the broken areas on the D455 depth images now rendered correctly?

     

    0
    Comment actions Permalink
  • Liam Neric

    Thank you for your quick answer Marty.

     

    The biggest depth problem is not under 1M, but between 1.5M and 3M distance.

     

    Here is the result with disparity shift of 200

     

    Does it require more fine-tuning to get the D455 to work in comparison to D415 and D435? I get the impression that I'm not the only customer that has difficulty with the depth quality of this camera.

     

    BR, Liam

     

     

    0
    Comment actions Permalink
  • MartyG

    The downside of Disparity Shift is that whilst increasing it above 0 reduces the minimum depth distance, increasing the value also progressively reduces the maximum observable depth range and strips out the background of the image, which looks as though what is happening to you when applying a DS of 200.

     

    Aside from improved depth accuracy over medium to long range (3 to 6 meters) and a wider field of view size, the D455's depth sensing should perform similarly to that of D435.

     

    Next, please try going to the Laser Power option under Stereo Module > Controls and setting it to its maximum value of '360' to see whether that helps to enhance the depth image.

     

    You can also try resetting the D455 to its factory-new default calibration values in the RealSense Viewer with the instructions at the link below.

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

    0
    Comment actions Permalink

Please sign in to leave a comment.