RealSense Support

Problems calibrating multiple d435 camera units

Comments

1 comment

  • MartyG

    Hi Hannes  With D435 cameras, depth is measured from the front of the camera.  You can choose to manually add -4.2 mm to depth measurements to obtain a 'ground truth' measurement from the sensor lens instead of the front glass.  It is not necessary to do so though, and using the default depth measurement from the front glass is fine.

     

    You can reset a camera to its default factory-new calibration in the RealSense Viewer tool using instructions at the link below.

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

    0
    Comment actions Permalink

Please sign in to leave a comment.