RealSense Support

i can not see rgb camera

Comments

3 comments

  • MartyG

    Hi Megan001222  Can you confirm please that you are enabling the camera in the RealSense Viewer's options side-panel by clicking on the red icon beside RGB Camera and not using the 'Add Source' button at the top of the panel.  If you only have one RealSense camera attached then Add Source would only list non-RealSense RGB cameras such as a laptop's built in webcam and show it as USB 2.1.

     

     

    Can you also confirm please which RealSense Viewer version you are using and what the current firmware driver version installed in your D435 is.

    0
    Comment actions Permalink
  • Megan001222

    I already clicked on the red button next to the RGB camera and didn't add any other sources. I checked it again, but it still only works stereo module.

    Rralsense Viewer version is 2.55.1.0
    firmware driver version is 5.16.0.1

    0
    Comment actions Permalink
  • MartyG

    As your depth stream is working, please try using the instructions at the link below to reset the camera to its default factory-new calibration settings in the RealSense Viewer.

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

    0
    Comment actions Permalink

Please sign in to leave a comment.