RealSense Support

Difference in left and right camera

Comments

1 comment

  • MartyG

    Hi Jaan Goyvaerts  The left and right infrared sensors do not have a master and slave arrangement, though the center-line of the left IR sensor is the default 0,0,0 origin point of the depth image.   The data sheet document for the 400 Series cameras provides the following information regarding how a depth frame is constructed using the left and right sensors.

    **********

    The left and right imagers capture the scene and send imager data to the depth imaging (vision) processor, which calculates depth values for each pixel in the image by correlating points on the left image to the right image and via the shift between a point on the left image and the right image.  The depth pixel values are processed to generate a depth frame.  Subsequent depth frames create a depth video stream. 

    0
    Comment actions Permalink

Please sign in to leave a comment.