RealSense Support

Remove IR filter on D401

Comments

1 comment

  • MartyG

    Hi Achmadpurnomo95  There has been one past case where a lens was successfully removed but the risk of damaging the sensor makes doing so not worth it unless you are prepared to write off the module if it fails.

     

    RealSense 400 Series cameras can also make use of visible ambient light in the scene to aid depth processing, so if the camera is being used indoors then adding additional visible illumination to the scene (such as with an external lamp) could be an alternative option.

    0
    Comment actions Permalink

Please sign in to leave a comment.