View my account

Failed to read busnum/devnum on D435i Camera

Comments

3 comments

  • MartyG

    Hi Kanakshilledar111  The error Failed to read busnum/devnum is a very rare one.  In the past it has usually occurred when using RealSense cameras with low-power computing boards that have been unable to supply the camera through the USB port with sufficient power to meet its needs. 

     

    A solution has been to use a mains electricity powered USB 3 hub and attach the camera to the hub instead of plugging it directly into the computing device's USB port.

    1
    Comment actions Permalink
  • Kanakshilledar111

    Alright! I tried connecting it to my laptop and it is working fine. So I will try to get a power USB 3 hub.

    You can mark the above comment as resolved!

    Thanks

     

    0
    Comment actions Permalink
  • MartyG

    You are very welcome.  I'm pleased that I was able to help.  :)

    0
    Comment actions Permalink

Please sign in to leave a comment.