RealSense Support

d455 Accuracy issues

Comments

3 comments

  • MartyG

    Hello, the missing depth data on the table area that the plant is resting in is likely because the table is dark gray / black in color.  This is because it is a general physics principle (not specific to RealSense) that dark grey or black absorbs light and so makes it more difficult for depth cameras to read depth information from such surfaces.  The darker the color shade, the more light that is absorbed and so the less depth detail that the camera can obtain.  Casting a strong light source onto such surfaces can help to bring out depth detail.

     

    The camera may also be having difficulty obtaining accurate depth information from the dark blue wall behind the plant, as the wall is not very far distant from the plant and so I would expect its depth colorization to be more light blue or yellow than red (which indicates far distance from the camera).

     

    Does the depth image improve if you change the depth scale value in the RealSense Viewer from its default value of 0.001 to 0.0001 please?  The link below describes how to change the depth scale in the Viewer.

    https://github.com/IntelRealSense/librealsense/issues/8228#issuecomment-766181076

    0
    Comment actions Permalink
  • 1095425988

    Hi
    So, the reason for this problem is that the stem of the plant is too smooth, too little texture, and the structured light camera has difficulty obtaining depth information? Can the sdk enhance the projected infrared speckle effect? Because I had the same problem with a distant white wall as the background. Is there any other solution?

    0
    Comment actions Permalink
  • MartyG

    You can increase the strength of the infrared dot projection by increasing the Laser Power setting from its default value of '156' to its maximum of '360'.  This makes the pattern more visible to the camera, aiding depth analysis.

    0
    Comment actions Permalink

Please sign in to leave a comment.