RealSense Support

The default depth distance range for the D435i camera depth map

Comments

2 comments

  • 2629590615

    How to change the detectable depth distance range of the D435i camera depth map using a python program?

    0
    Comment actions Permalink
  • MartyG

    Hi, the minimum depth sensing distance of the D435i camera model will be around 0.1 meters / 10 cm.

     

    Below is an example of Python code for altering the minimum depth sensing distance with the Disparity Shift option.  As the Disparity Shift value is increased, minimum distance reduces but the maximum observable depth distance also reduces.  '100' is a good value to test with.

     

    device = rs.context().query_devices()[0]
    advnc_mode = rs.rs400_advanced_mode(device)
    depth_table_control_group = advnc_mode.get_depth_table()
    depth_table_control_group.disparityShift = 100
    advnc_mode.set_depth_table(depth_table_control_group)

     

    Using aligned data will not affect the depth range.

    0
    Comment actions Permalink

Please sign in to leave a comment.