RealSense D405 Depth Map Fidelity
Hi there, I am using the D405 depth camera to track a marker that I detect using OpenCV. I have a green marker that I track by masking a camera image, then I use the tracked position to retrieve 3D coordinates within the depth matrix.
However, when I visualize the depth map through my own code, it seems like the map has a lot more "dead zones".

However, when I view through the realsense viewer, it seems as though there are less dead zones. Is there any way I can improve this?

I am sensing at a range of 175mm away from my markers. From documentation the D405 is supposed to sense at distances as small as 70mm.
Thanks,
Kenneth
-
For a 1:1 comparison, here is the head in the same position and sensed through my code in the API.

And here is my code:
import pyrealsense2 as rs
import cv2
import numpy as np
import library as lib
import matplotlib as plt
import os, psutil
import time
#--------------------------------------------------------------------------------------------- FILE PATHS --------------------------------------------------#
output_file = '405test.txt' #your txt filename
if os.path.exists(output_file):
with open(output_file, 'w') as f:
f.write('')
f.close()
calibration_file = 'color_calibration\color_calibration_values.txt'
#--------------------------------------------------------------------------------------------- DEFINING SETUP PARAMETERS --------------------------------------------------#
color_res= [1280, 720] ; depth_res= [1280, 720] ; fps=30
pipe = rs.pipeline() ; cfg = rs.config()
pc = rs.pointcloud()
df = rs.decimation_filter()
colorizer = rs.colorizer()
cfg.enable_stream(rs.stream.color, color_res[0],color_res[1], rs.format.bgr8, fps)
cfg.enable_stream(rs.stream.depth, depth_res[0], depth_res[1], rs.format.z16, fps)
color_path = '405test.avi'
depth_path = '405test.avi'
colorwriter = cv2.VideoWriter(color_path, cv2.VideoWriter_fourcc(*'XVID'), fps, (color_res[0],color_res[1]), 1)
depthwriter = cv2.VideoWriter(depth_path, cv2.VideoWriter_fourcc(*'XVID'), fps, (depth_res[0],depth_res[1]), 1)
profile = pipe.start(cfg)
depth_sensor = profile.get_device().first_depth_sensor()
#Controlling Depth Sensor Options
if depth_sensor.supports(rs.option.depth_units):
depth_sensor.set_option(rs.option.depth_units,0.0001)
# depth_sensor.set_option(rs.option.laser_power, 360)
align_to = rs.stream.color
align = rs.align(align_to)
#Initializing marker objects
marker1 = lib.marker()
marker2 = lib.marker()
counter = 0
start_time = time.time()
while True:
#Incrementing Counter
counter += 1
print('counter: ' + str(counter))
#Aligning depth and color frames
frame = pipe.wait_for_frames()
aligned_frames = align.process(frame)
aligned_depth_frame = aligned_frames.get_depth_frame()
aligned_color_frame = aligned_frames.get_color_frame()
if not aligned_depth_frame or not aligned_color_frame:
continue
#Defining depth_image
depth_image = np.asanyarray(aligned_depth_frame.get_data())
color_image = np.asanyarray(aligned_color_frame.get_data())
depth_cm = np.asanyarray(colorizer.colorize(aligned_depth_frame).get_data())
#mapping point cloud to color frame and calculating the d
# epth frame
pts = pc.calculate(aligned_depth_frame)
pc.map_to(aligned_color_frame)
track = []
track,detected = lib.detect_color_marker(color_image,calibration_file,visualize=True) #Set number to manipulate exposure
print(detected)
if detected==True:
vtx = pts.get_vertices()
vertices = np.asanyarray(vtx).view(np.float32).reshape(-1,3) #Reshaping for xyz
length1 = lib.pass_coordinate(track[0][0], track[0][1], depth_res[0]) #Retrieving pixel number to pass to depth matrix
position1 = vertices[length1]
print(position1) #Retrieving XYZ position1
marker1.filter(position1)
current_time = time.time()
position1 = np.append(position1, format(current_time - start_time,'.6f'))
length2 = lib.pass_coordinate(track[1][0], track[1][1], depth_res[0]) #Retrieving pixel number to pass to depth matrix
position2 = vertices[length2] #Retrieving XYZ position1
marker2.filter(position2)
current_time = time.time()
position2 = np.append(position2, format(current_time - start_time,'.6f'))
if marker1.state is True and marker2.state is True:
with open(output_file,"a") as f:
f.write('A: ' + str(position1) + ' ' + 'B: ' + str(position2) + '\n')
f.close()
else:
print('not detected')
#writing out to video
colorwriter.write(color_image)
depthwriter.write(depth_cm)
cv2.circle(color_image,(int(color_res[0]/2),int(color_res[1]/2)), 5, (0,0,255), -1)
cv2.circle(depth_cm,(int(depth_res[0]/2),int(depth_res[1]/2)), 5, (0,0,255), -1)
##Show stream
cv2.imshow('rgb', color_image)
cv2.imshow('depth', depth_cm)
key = cv2.waitKey(1) # Wait Esc key to end program
if key == 27:
break
colorwriter.release()
depthwriter.release()
pipe.stop() -
Hi Kvuong The RealSense Viewer tool applies a range of image-improving post processing filters that are enabled by default in the Post Processing section of the Viewer's options side-panel. A script, like the one that you wrote, has no filters enabled by default and they must be deliberately programmed into the script in order to obtain results that are closer to the depth image that is output by the Viewer.
The link below has a simple Python example of using alignment with a Decimation post-processing filter.
https://github.com/IntelRealSense/librealsense/issues/2356#issuecomment-465766323
The D405 camera's ideal depth sensing range is between 7 cm (70 mm) and 50 cm (500 mm). So 175 mm (17.5 cm) is well within the D405's ideal range for a good depth image.
-
The link below has Python code for setting up decimation, spatial and temporal filters.
https://github.com/IntelRealSense/librealsense/issues/10078#issuecomment-997292916
Please sign in to leave a comment.
Comments
6 comments