RealSense Support

Frame Drop issue

Comments

3 comments

  • MartyG

    Hi Sundaramoorthi S  Usually, only one RealSense camera per Raspberry Pi board is used, like in the image below.  There are single-board computers that are better suited to having two RealSense cameras attached and active simultaneously, such as Up Squared and Nvidia Jetson.

     

     

    You could check whether your issue might be caused by two cameras over-burdening the Pi's CPU by having just one camera attached and seeing whether the Pi's temperature is still 85 degrees.

     

    Another possibility would be a bad USB cable causing overheating of the camera by supplying too much power, and some of that heat getting passed back to the Pi.  An easy way to check for overheating is to let the camera run for a few minutes after start-up and then touch the camera casing.  If it is hot to the touch then it is likely overheating.

    0
    Comment actions Permalink
  • Sundaramoorthi S

    Hi MartyG,

    When using a single Intel RealSense D410 with a Raspberry Pi, we've observed that the ASIC temperature of Intel realsense D410  is maintained at 50 degrees Celsius. We are concerned about whether this will impact the sensor's performance. 

    0
    Comment actions Permalink
  • MartyG

    50 degrees C is not ideal.  Above 42 degrees there will be an increased risk of the image being negatively impacted.  The laser safety mechanism will not turn off the camera's laser unless the projector temperature exceeds 60 degrees C though.  The camera can continue to operate with the laser disabled but depth image quality would likely reduce and the infrared image become darker.

     

    You could investigate the possibility of adding a heat sink component to the back of the D410.  This is a block of metal that draws heat away from electronics, such as the D410 board.  Page 119 of the current edition of the data sheet document for the 400 Series cameras provides advice about heat sinks.

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

    0
    Comment actions Permalink

Please sign in to leave a comment.