RealSense Support

Intel D457 Hardware and Software Interfacing

Comments

2 comments

  • MartyG

    Hi Gatordevin  Yes, I can confirm that the FAKRA connection does not operate when the mode switch is set to USB, and the camera is detected and operates as D455 instead of D457.  In USB mode it is not necessary to use the special driver and the deserializer board that a FAKRA connection requires.

     

    It would be possible to create a custom waterproof housing to place a D455 camera in, like the example below from an underwater project, though using a D457 in USB mode would be much easier.

     

    1
    Comment actions Permalink
  • Gatordevin

    Awesome! Thank you so much for the response. I will also report back here if it works with the Java library for others but based on what you described it sounds like it should be perfect.

    0
    Comment actions Permalink

Please sign in to leave a comment.