RealSense Support

alignment of D435i in Labview

Comments

1 comment

  • MartyG

    The intrinsics of the target stream should be used.  So if you are aligning depth to color (and so color is the target stream) then you should use the color intrinsics.  This is because when depth is aligned to color, the 0,0,0 world-space depth origin becomes the center-line of the RGB sensor.

     

    In an unaligned image, the 0,0,0 depth origin is the center-line of the left IR sensor.

    0
    Comment actions Permalink

Please sign in to leave a comment.