RealSense Support

Object Recognition Using the D435i

Comments

3 comments

  • MartyG

    Hi, When you say that the angle of your camera is biased, do you mean that it is tilted strongly up or down?  It is fine to tilt RealSense 400 Series cameras up to 30 degrees in the up or down direction, but beyond that angle (such as 40 degrees or more), problems may manifest in the depth sensing.  The camera can be pointed 90 degrees up or down without problems though.

     

    The RealSense SDK does not have built-in object detection.  A third-party tool called YOLO is commonly used with RealSense cameras for that application.

    0
    Comment actions Permalink
  • 815613232

    Sorry, I may not have described it clearly.
    At present, we cannot accurately identify the centroid of the object through the yolo algorithm. It may be because of the perspective problem that the recognized centroid of the bounding box is not the real centroid of the object. Can you provide a method to calculate the centroid of the object through the three-dimensional bounding box.

    0
    Comment actions Permalink
  • MartyG

    Typically when a 3D bounding box needs to be generated, I recommend that YOLO is used in conjunction with darknet_ros_3d.

     

    darknet_ros

    https://github.com/leggedrobotics/darknet_ros

     

    darknet_ros_3d

    https://github.com/IntelligentRoboticsLabs/gb_visual_detection_3d

     

    If you already have a 3D bounding box and believe that inaccurate hand-eye calibration may be the issue then you could explore the RealSense-compatible hand-eye calibration methods highlighted in the link below.

    https://github.com/IntelRealSense/librealsense/issues/11736#issuecomment-1525124566

    0
    Comment actions Permalink

Please sign in to leave a comment.