4 CAM D430 Setup with USB2 Hub
We are testing 4 cam D430 setup with an externally powered USB2 Hub. We have tested different types of these USB hub and in all cases, we are facing the same issue that at any time only three of those 4 cams are working. Resolution is set to 640*480 and we have tried at 30 and 15 fps.
MartyX Grover any help is this regard will be appreciated. Do you have any recommendation for any USB2 hub which can handle 4 d430 cams at once?
-
Hi Deepak Kumar In Intel's multiple camera white-paper document they tested up to 4 cameras with the AmazonBasics powered USB3 model. I used an AmazonBasics hub myself with RealSense cameras based on that recommendation and have never had problems with it over a period of years.
You should choose a hub that supports 5 gigabits per second bandwidth. Each camera will consume a certain amount of bandwidth, and you need a large enough total bandwidth allowance to handle the bandwidth consumption of 4 cameras simultaneously. At low 640x480 resolution, a 5 Gbps bandwidth should be sufficient for handling the data of all those cameras.
If you cannot find a suitable USB2 hub, a solution may be to obtain a USB3 hub and use USB2 cables with the cameras so that they are detected as USB2 devices. A device on a USB2 cable cannot be detected as USB3 because USB2 cables lack some extra wires inside them that enable USB3 speed.
If your project requires a USB2 hub and you would like to follow the AmazonBasics recommendation, this brand is usually USB3 but there is a USB2 model that is findable if you search for amazonbasics hub 7 port tower
-
MartyG , Thanks for the reply. I will follow your suggestions and update.
Have you ever tried the 4 cam setup with a USB2 Hub ?
-
Hi MartyX Grover , upon further testing with externally powered USB2 hub, we are facing some issues. All the 4 vision processors in our setup are not working and they are overheating. Is there a forum or support from INTEL for users facing this issue with overheating of vision processors. Is there any repair or exchange service offered?
-
Hi Deepak Kumar Intel do not offer a repair service for RealSense products. If they were recently purchased then you may be able to return them to the retailer that you purchased them from.
Overheating might be caused by a bad USB cable or a glitch on the USB port. If you are using a hub and the overheating occurs on all ports then it might be more likely to be a cable quality issue. You said in your opening comment though that 3 of the 4 D430 were working. Does the overheating issue only occur with USB2 hubs or does it also occur if you plug the camera directly into the computer?
Conceivably heating could also occur if the powered hub was having excess mains electricity delivered to it, which could account for all ports on the hub having the issue. Is the casing of the hub hot to the touch during use?
-
Intel do not provide a repair service for RealSense hardware products.
I am not a member of the support team on this Intel RealSense Help Center site, I volunteer here. I will highlight your case to the Help Center support team so that they can provide you with advice about your situation.
-
Thank you MartyG for your effort and time. I really appreciate it.
Please sign in to leave a comment.
Comments
12 comments